Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 March 2021Siemens Mobility GmbH and Infineon Technologies AGMunich
Sustainable operation of trains: Power-efficient on-board electrical system uses technology developed by Siemens Mobility and Infineon
“Our vehicles should not only offer the highest level of passenger comfort but also enable our customers to operate them sustainably over the entire product life cycle. Energy-efficient on-board train power systems can make a major contribution to economical and environmentally-friendly train operations,” said Albrecht Neumann, CEO of Rolling Stock at Siemens Mobility.
Siemens Mobility uses the new converter for various train platforms. As a result, the platforms are maintenance-friendly, reliable, economical and, above all, power efficient. “With SiC, we achieve higher switching speed as well as efficiency to reduce the size of transformers, capacitors, cooling elements and the housing unit. The advantages of this semiconductor material are evident and are now being leveraged in rail-bound vehicles,” said Dr. Peter Wawer, President of Infineon's Industrial Power Control Division.
In addition to providing the AC voltage (e.g., 3 AC 400 V 50 Hz) required for the vehicle power system, auxiliary converters also deliver the required battery voltage (e.g., 110 V DC). To achieve this, they convert the DC voltage provided at the converter input. They ensure that train passengers can charge laptops and smartphones; the air conditioning and ventilation systems are running; and the on-board restaurant can offer hot and cold drinks and food. Without them, connectivity, information or entertainment services on trains would not be available. As part of the system, SiC reduces the overall costs in the on-board electrical system and the energy consumption of the auxiliary converter. It also enables more compact and lighter converter designs, along with a modular and service-friendly design to ensure lower maintenance costs.
The auxiliary converter makes use of power semiconductors in a half-bridge topology that are based on Infineon's CoolSiC™ MOSFET 1200 V technology. Depending on the design, 8 to 16 half-bridge modules are installed for each converter.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2020, which ended on September 30, 2020, Siemens Mobility posted revenue of €9.1 billion and had around 38,500 employees worldwide. Further information is available at:
www.siemens.com/mobility.
Contact
Eva Haupenthal
Siemens Mobility GmbH
Otto-Hahn-Ring 6
81739 Munich
Germany
81739 Munich
Germany
+49 152 01654597