[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release17 November 2020Digital IndustriesNuremberg
Siemens presents first industrial 5G router
Growing demand for remote access via public 5G networks for remote maintenance
Scalance MUM856-1 connects local industrial applications to the public 5G network
Sinema Remote Connect management platform provides secure access to remote plants and machines
Siemens presents the first industrial 5G router for connecting local industrial applications to a public 5G network. The device will be available in spring 2021. Using the newly developed Scalance MUM856-1, industrial applications such as machines, control elements, and other devices can be accessed remotely via a public 5G network, providing a simple remote maintenance option for these applications using the high data rates offered by 5G. The Sinema Remote Connect management platform for VPN connections can be used to provide easy and secure access to these remote plants or machines – even if they are integrated in other networks.
Growing demand for remote access via public 5G networks for remote maintenance
Scalance MUM856-1 connects local industrial applications to the public 5G network
Sinema Remote Connect management platform provides secure access to remote plants and machines
Siemens presents the first industrial 5G router for connecting local industrial applications to a public 5G network. The device will be available in spring 2021. Using the newly developed Scalance MUM856-1, industrial applications such as machines, control elements, and other devices can be accessed remotely via a public 5G network, providing a simple remote maintenance option for these applications using the high data rates offered by 5G. The Sinema Remote Connect management platform for VPN connections can be used to provide easy and secure access to these remote plants or machines – even if they are integrated in other networks.
In industry, in addition to the
need for local wireless connectivity, there is increasing demand for remote
access to machines and plants. In these cases, communication needs to bridge
long distances. Public mobile networks can be used to access devices that are
located at a considerable distance, for example in other countries. In
addition, service technicians can connect to the machines they need to service
via the mobile network while on the go.
Public 5G networks are
therefore an important element of remote access and remote maintenance
solutions. They can be used, for example, to provide users with very high
bandwidths in urban areas with small radio cells and high frequencies. In rural
areas, radio cells have to cover a large area, which is why lower frequencies
are used. Particularly at the edges of radio cells, for example for LTE or
UMTS, there are often significant losses in terms of both the bandwidth and
stability of the communication connection. And it is exactly in these remote
areas where stable bandwidth transmission is required for remote maintenance or
video transmission, for example for water stations. With innovative 5G
communications technologies, considerably more bandwidth with greater
reliability is available at the edges of radio cells and the average data rate
for users within a radio cell increases. The new Scalance MUM856-1 also
supports 4G so that operation is possible even if a 5G mobile network is not
available. The device can also be integrated in private local 5G campus
networks. Siemens is testing this use case in their own Automotive Test Center
in a private standalone 5G test network, which is based on Siemens components. There,
automated guided vehicle systems are connected using 5G in order to test
current and future industrial applications and to drive forward the use of 5G
technology in industry.
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.