[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release14 July 2020Digital IndustriesNuremberg
Flexible process design at machine and line
level
New plant intelligence options for the control and monitoring of recipe-controlled processes
Easy orchestration of production sequences with “WinCC Unified Line Coordination” (LCS)
Quick changes to processes in recipe and sequence-based production with “WinCC Unified Sequence” (SES)
Siemens is expanding its offer for the Simatic WinCC Unified visualization system to include two new plant intelligence options: Line Coordination (LCS) and Sequence (SES) enable the fast orchestration and adaptation of production sequences for the control and monitoring of recipe-controlled processes, such as those used in the food and beverages industry. With these new software options, users can flexibly design production sequences, monitor different plant sections and therefore utilize the capacity of individual production machines better and more evenly, increasing both effectiveness and economic efficiency. For both SES and LCS, Siemens supplies automation modules and the corresponding controls for the visualization, which can be engineered in the Totally Integrated Automation (TIA) Portal engineering framework. Production sequences can be parameterized with the corresponding modules, which eliminates programming effort and reduces engineering effort. The two new plant intelligence options can be combined to meet the relevant requirements.
New plant intelligence options for the control and monitoring of recipe-controlled processes
Easy orchestration of production sequences with “WinCC Unified Line Coordination” (LCS)
Quick changes to processes in recipe and sequence-based production with “WinCC Unified Sequence” (SES)
Siemens is expanding its offer for the Simatic WinCC Unified visualization system to include two new plant intelligence options: Line Coordination (LCS) and Sequence (SES) enable the fast orchestration and adaptation of production sequences for the control and monitoring of recipe-controlled processes, such as those used in the food and beverages industry. With these new software options, users can flexibly design production sequences, monitor different plant sections and therefore utilize the capacity of individual production machines better and more evenly, increasing both effectiveness and economic efficiency. For both SES and LCS, Siemens supplies automation modules and the corresponding controls for the visualization, which can be engineered in the Totally Integrated Automation (TIA) Portal engineering framework. Production sequences can be parameterized with the corresponding modules, which eliminates programming effort and reduces engineering effort. The two new plant intelligence options can be combined to meet the relevant requirements.
With WinCC Unified Line Coordination, recipe and batch-controlled production processes can be automated in the TIA Portal. Production sequences for networked machines in the production line can be coordinated, synchronized and monitored using a Simatic S7-1500 controller and WinCC Unified. The new software option is tailored to the technological requirements of different processes through the relevant standard functions. For example, for plants in the TIA Portal based on ISA-88 - the standard for batch processing control - users can structure in line with a technological hierarchy and standardize production processes using a recipe system. To support this, the software package includes the necessary engineering and runtime components for recipe management as well as control elements for the visualization. Monitoring options offer improved transparency and monitoring of planned or current production processes. In the current version, LCS supports production sequences which are programmed in a Simatic S7-1500 controller or in WinCC Unified Sequence (SES).
With the Sequence (SES) plant intelligence option, users can flexibly design and automate individual production steps at machine and plant section level. This means that production sequences and parameters can be adjusted at any time - even during operation - without making changes to the PLC program: the operator can manually access the automatic sequence online and jump to another step or adjust setpoints as required. This may be necessary, for example, due to variations in feedstock or in general if a different sequence for individual production steps is required for flexible paths through production. The new software option meets real-time requirements because the sequencers are executed on the Simatic S7-1500 controller and therefore support reliable plant operation and a high level of system availability. The new software option is also based on standardized production sequences as per ISA-88 and can be scaled for small or large plants thanks to the range of module sizes. The pre-built visualization control and the function modules supplied in the TIA Portal ensure a high degree of engineering efficiency by reducing commissioning and test times for the user.
Line Coordination
(LCS) and Sequence (SES) enable the fast orchestration and adaptation of
production sequences for the control and monitoring of recipe-controlled
processes
Note: The Siemens Digital
Enterprise Virtual Summit will be held on July 16, 2020 and will include breakout
sessions on Simatic WinCC Unified.
To get access as a media representative,
please register here.
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet www.siemens.com.