[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
One-stop shop – RWE invests in new control system for power plants
System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.
System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.
The new technology will be used in the RWE Supply & Trading Dispatch Centre on Europe's largest trading floor, which is located in Essen. This is where the central command and control operations of all RWE plants in Europe are located. A wall of monitors several metres high and wide shows in real time which RWE power stations are feeding power into the grid, the feed-in levels, and which plants are being ramped up or down. Engineers sit in front of the screens and optimise all of RWE's conventional power generation assets around the clock. A powerful command and control system is crucial to this task.
By connecting numerous small units, RWE aims to create a virtual power plant in order to advance the energy transition. The conventional power stations and pumped-storage plants offset the volatility of renewables, and thanks to state-of-the-art technology, can be controlled down to the second. Even the requirements of transmission system operators with respect to system services, grid disturbances and minimisation of balancing energy are optimally met.
Optime, a new SCADA system, gives RWE state-of-the-art unified control technology and saves both infrastructure and service costs. The new system is based on Siemens Spectrum Power.
Guido Hommelsheim, Head of Dispatch at RWE Supply & Trading, is pleased: “Optime gives us automatic control in real time as well as improved control performance. In addition, it allows us to better coordinate our portfolio, which consists of renewable energy plants, the existing flexibilities of our industrial customers, and conventional power stations. In view of the expansion of renewable energy, this is becoming increasingly important.”
The RWE control team keeps constant watch over developments as they unfold because power supply and demand can deviate from projections, for example in the event of unusual weather conditions or major events. In such cases, the engineers working in the Dispatch Centre must respond quickly. Up to 500 optimisation runs are performed every day using the power plant dispatch optimisation program developed specifically for this purpose by experts at RWE. This program determines the most economical use of all power plant units and machines and uses that data to create current target schedules. These are then transmitted via Optime as a target figure to the corresponding unit or machine control system of each power plant location.
Sabine Erlinghagen, CEO of Siemens Digital Grid, says “The success of this project hinged on the close cooperation between RWE and Siemens. The new control technology for Europe’s largest trading floor enables Siemens to combine state-of-the-art control software and SCADA tools on a single platform. This helps RWE to better coordinate generation capacities in Germany, the Netherlands and Belgium. At the same time, high-quality, virtually disruption-free system services can be provided. In the future, it will be possible to optimise the integration of fluctuating levels of renewables-based energy. This holistic approach to power plant management will make a contribution to accelerating the energy transition in Europe and the world.”
The new control technology based on Siemens Spectrum Power supports the integration of other equipment such as batteries and diesel-powered emergency power units. By connecting numerous smaller plants, RWE aims to create a virtual power plant in order to advance the energy transition.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
RWE Supply & Trading GmbH RWE Supply & Trading is the interface between RWE and the energy markets around the world. Approximately 1,600 employees from 40 countries trade electricity, gas, commodities and CO2 emission allowances. Accurate market analyses and a high degree of customer centricity enable them to create innovative energy supply solutions as well as risk management concepts for industrial operations. The trading company also ensures the commercial optimisation of power plant dispatch at RWE, operates natural gas storage systems and markets electricity from renewables.