Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 November 2019Digital IndustriesNuremberg
Siemens presents new version of Braumat process control system
In order to enhance the reporting options, a batch report with a basic choice of process parameters has been integrated. Users can now create reports with the help of MS Excel. Braumat V8.0 is also now connected to the established PM-Quality option. This means that MES (Manufacturing Execution System) and MIS (Management Information System) functions are now available for calculating KPIs (Key Performance Indicators) such as plant availability. In the new version, storage location management is integrated together with dosage management in the recipe system, enabling the efficient and flexible automation of mixing processes. Recipes are automatically adjusted according to storage location availability and the quantity specifications of the batches to be produced. High-precision, self-optimizing weighing operations are fully automated with the integrated Siwarex weighing system. The Braumat V8.0 process control system continuously checks recipes and quantities for the individual production processes, thus reducing overdoses of malt, hops and diatomaceous earth. A combination of password protected Simatic S7-1500 controllers, encrypted communication on the terminal bus as well as extended user management and company ID registration via an RFID card reader increases security during the production sequences.
Siemens is presenting its new version 8.0 of the Braumat brewery process control system at the BrauBeviale in Nuremberg.
New Braumat V8.0 is available in both a standard and lean edition: With Braumat Lean, micro breweries and craft brewers can benefit from process automation from just a quantity of four units and one Simatic Open Controller. This can be expanded up to 40 units as required. Braumat Lean can also be operated as a compact, single user station or for remote areas of large breweries, such as laboratories. With the Standard edition, it is possible to create complex plant structures with redundant client-server features and server visualization. The Lean Edition of Braumat V8.0 can be expanded to the Standard Edition. After just a few days of training, users are able to configure new Braumat plants. For other food and beverage sectors such as dairies, cheese factories or soft drinks, the Sistar version 8.0 process control system is available.
As a long-term partner in the international brewing and beverages industries, Siemens is demonstrating at this year's BrauBeviale being held in Nuremberg from November 12 through 14 how its innovative brewery automation processes enable the first step into digitalization. Visitors to booth 419 in hall 7 can experience the path to digitalization themselves: Exhibits stretch from the lean version of the Braumat process control system for the automation of micro breweries, to a standard Braumat system with a Manufacturing Operation Management (MOM) solution and energy management, to cutting-edge technologies such as cloud and edge computing.
For this press release
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at
www.siemens.com
.
Contact
Julia Kauppert
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (174) 311-8098