Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 October 2019Siemens Mobility GmbHSingapore
Siemens Mobility to set up Singapore’s Downtown Line signalling simulation center
The DTL is one of Singapore’s longest mass transit lines – with nearly 42 kilometers of track and 34 stations from Bukit Panjang in the north-west to Expo in the east, with a daily ridership of more than 500,000. When its expansion is completed in 2024, it will be 44 kilometers long with an additional three stations. The test center, which will be ready by end of 2020, will enable testing and integration of the DTL’s signalling system before these three new stations commence operations. The test center will be located in Gali Batu Depot, where the DTL’s operation control center is housed.
DTL currently uses Siemens Mobility’s signalling system and automatic train operations. The test center will be a digital twin of DTL’s signalling system, with capabilities to test key hardware interfaces. It will digitally simulate these operations to eliminate any risks of service disruptions during system enhancements, troubleshooting, vulnerability checks, system patching, as well as allow testing of new software releases prior to deployment. It will also allow hands-on trainings and thus boost operations and maintenance competency.
“Singapore is at the forefront of mass transit technology. By utilizing digitalization, LTA’s operations will see greater availability and reliability. Data analytics and preventive failure prediction that was previously done on the lines will now be done remotely and digitally, without impacting operations or passenger service”, said Michael Peter, CEO of Siemens Mobility.
The test center will include hardware similar to the rest of the system, including:
- WESTRACE MKII interlocking, Trackside TRAINGUARD Communications-Based Train Control (CBTC) System and radio network equipment;
- Trainborne TRAINGUARD CBTC System;
- RAIL9000 Automatic Train Supervision (ATS) System in Depots and Operation Centres
The test center will be established in two stages and completed by end-2020. The first will include ATS simulation environment and the second will include the full test environment: CBTC, interlocking, communications and trackside elements.
Siemens Mobility is playing an important role in transforming Singapore’s transportation infrastructure. In addition to the signalling and test center for DTL, it will also provide electrification for two other mass transit projects: Circle Line Stage 6 and North East Line extension. The company also operates one of its digital labs in Singapore, transforming the future of road traffic and is conducting extensive autonomous driving research with its partner CETRAN.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal 2018, which ended on September 30, 2018, the former Siemens Mobility Division posted revenue of €8.8 billion and had around 34,200 employees worldwide. Further information is available at:
www.siemens.com/mobility.
Contact
Kara Evanko
Siemens Mobility GmbH
One Penn Plaza
New York, NY 10119
USA
New York, NY 10119
USA
+1 (202) 285 3072