Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release16 September 2019Digital IndustriesHanover
Siemens extends Sinumerik Edge to include more applications, bringing artificial intelligence to machine tools
Siemens has extended its machine-oriented Sinumerik Edge to include new applications. At EMO 2019, Siemens is presenting the Analyze MyWorkpiece /Vision Edge application. The software is based on artificial intelligence and detects whether the right workpiece is in the correct position.
Using Analyze MyWorkpiece /Vision to reduce downtimes based on artificial intelligence
At EMO 2019, Siemens will present the Analyze MyWorkpiece /Vision Edge application for the first time. The software works with image recognition and is based on artificial intelligence. It detects whether the right workpiece is in the correct position in the machine room– and it works better than the human eye. If the workpiece is positioned correctly, processing can be started. The application can also detect wear on the tool. In addition, the application transmits the work process live via camera from the machine room and documents all image data. Analyze MyWorkpiece/Vision ensures preparation and process quality for users. By detecting tool wear, resources can be used efficiently. The application configuration is tailored to the machine operator, meaning that users can benefit from artificial intelligence without a great deal of expert knowledge. Job setup using the application is also very easy, so an easy integration into the manufacturing process is possible. Analyze MyWorkpiece /Vision joins the portfolio of existing applications such as Analyze MyWorkpiece /Toolpath, Analyze MyWorkpiece /Capture and Analyze MyWorkpiece /Monitor, all of which contribute to better workpiece and process quality, helping to increase the productivity of machine tools and to reduce costs.
Increased machine productivity using artificial intelligence with Optimize MyMachining /Magazine
In the field of performance enhancement, Siemens is also presenting a new Edge application at this year
's EMO. Part of the performance increase results from an optimal arrangement of tools in the magazine. The optimization algorithm of Optimize MyMachining /Magazine is based on artificial intelligence and runs on Sinumerik Edge. It calculates the tool arrangement in order to minimize manufacturing time. In the field of improved machine productivity, the new application adds to the Optimize MyMachining /Trochoidal Edge application presented at last year
's AMB.
Protect MyMachine /3D Twin for Sinumerik One
The Sinumerik Collision Avoidance application will be presented at this year
's EMO as an Edge-based application especially for Sinumerik One. Protect MyMachine /3D Twin includes comprehensive protection of the machine and tools in terms of the current setup situation, including dynamic observation of workpiece protection. By using Sinumerik Edge the performance and productivity of the NCU is not adversely affected by additional computing performance. With Create MyVirtual Machine and Run MyVirtual Machine – both software applications for Sinumerik One for creating digital twins – computational models created in this context can be used to include in Protect MyMachine /3D Twin. Protect MyMachine /3D Twin joins the existing AnalyzeMyMachine /Condition Edge application in the field of digitalization solutions for machine tool condition monitoring.
Edge Management as a control center
With Manage MySinumerik Edge, Siemens is presenting its Industrial Edge Management solution to manage Edge applications for machine tools for the first time at EMO 2019. With Manage MySinumerik Edge, all connected Edge devices can be administered, monitored and updated centrally. In addition, Edge applications are always distributed in the latest version efficiently and securely to Sinumerik Edge devices. Applications can be installed on Sinumerik Edge devices without adverse effects, regardless of the machine tool operating state. Edge applications for Sinumerik Edge can be provided both by Siemens and by third-party suppliers. Thus, users and machine builders can develop own applications, which are tailored to the individual requirements of their machines. In the future, Edge applications can be offered via a marketplace in MindSphere. The operating system of the Sinumerik Edge is integrated in a holistic security concept. It enables the stable operation of one or more applications in parallel and provides a secure software environment for the execution of applications on Edge devices.
For further information regarding Siemens at the EMO 2019, please see
www.siemens.com/press/emo2019 and www.siemens.com/emo
For further information regarding Sinumerik Edge, please see www.siemens.com/industrial-edge
www.siemens.com/press/emo2019 and www.siemens.com/emo
For further information regarding Sinumerik Edge, please see www.siemens.com/industrial-edge
For this press release
Social Media
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI's unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.
Contact
Katharina Lamsa
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975