Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
Siemens modernization and upgrade services can breathe new life into existing power generating assets.
Siemens recently signed an agreement with Shanghai Shenergy Energy Technology Co., Ltd. (Shenergy Technology) to implement a high-temperature subcritical upgrade for a 320MW steam turbine unit at Xuzhou Power Plant, a subsidiary of China Resources Power Holdings Co., Ltd (CR Power) in Jiangsu province. It is estimated that the upgrade will enhance the unit's power output efficiency up to 42.9 percent, reduce its emissions by more than 10 percent and extend its overhaul interval from six to 12 years. This will increase the generation revenue of the plant while reducing maintenance costs significantly. The project is expected to be concluded in mid-2019.
"We are glad to bring proven technologies and experience in steam turbine modernization and upgrades to China for making the thermal power of the country more efficient and contribute to the emission reduction targets set by the government," said Gery Nocker, Executive Vice President of Siemens Ltd., China and General Manager of the Power Generation Services Division.
Steam temperature is the key factor in influencing the power generation efficiency and coal consumption of a steam turbine. In this project, the main steam and hot reheat steam temperature will be raised from 537 to 600 degrees. In addition, the project will include adopting control stage, advanced blade designs, such as 3DS and 3DV blades, and additional steam extraction for the A0 high-pressure pre-heater. This will help CR Power to lower the coal consumption of the subcritical unit by more than 10 percent to 287g/kWh, which is close to the ultra-supercritical level. The project will also help reduce performance degradation while improving the unit's flexibility, availability and reliability.
Professor Feng Weizhong, General Manager of Shanghai Shenergy Power Technology Co., Ltd. said, "Although we are experiencing energy transition right now, coal-fired power generation is still the backbone of the energy mix in China. This poses high requirements on the coal fired power plants in service, and the market demand for upgrade solution increases accordingly. As can be seen from technical strength, practical experience and 20 years of fruitful cooperation, Siemens is our trustworthy partner."
Over the past 36 years, Siemens has successfully upgraded more than 300 large scale steam turbines worldwide. Moreover, Siemens' four service centers in Beijing, Huludao, Shanghai and Yixing together with nearly a hundred engineers is part of a global network of over 80 service centers that offers Chinese customers state of the art technical and service support solutions.​

Further Information

Contact

Amy Pempel

Gas and Power

+1 (407) 408-1932

Link to this page
www.siemens.com/press/energyservice-china