[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Operator TriMet relies on rail technology from Siemens for newly opened light rail line
MAX Orange Line between Portland and Milwaukie
18 light rail vehicles S70 type energy
Energy storage system type Sitras SES
Signaling and communication system
Today, TriMet's new MAX Orange Line, a light rail project between Portland and Milwaukie (USA), was officially inaugurated. Siemens advanced rail technologies are now operating on the Orange line including its S70 light rail vehicles designed and manufactured at Siemens Sacramento, California plant to move riders along the system, rail signaling and communication systems to help manage train operation, and the company's first Sitras SES energy storage unit in the U.S. that uses regenerative braking to sustainably power the line.
MAX Orange Line between Portland and Milwaukie
18 light rail vehicles S70 type energy
Energy storage system type Sitras SES
Signaling and communication system
Today, TriMet's new MAX Orange Line, a light rail project between Portland and Milwaukie (USA), was officially inaugurated. Siemens advanced rail technologies are now operating on the Orange line including its S70 light rail vehicles designed and manufactured at Siemens Sacramento, California plant to move riders along the system, rail signaling and communication systems to help manage train operation, and the company's first Sitras SES energy storage unit in the U.S. that uses regenerative braking to sustainably power the line.
New rail project between Portland and Milwaukie (USA)
The 7.3-mile (around 12 Kilometer) MAX Orange Line is the region's sixth construction project of the development project Metropolitan Area Express (MAX) to expand the city's transport network to cope with the expected population growth in the Portland area. The line will improve transit in the corridor that extends from the terminus of the MAX Green and Yellow lines at Portland State University in Downtown Portland to Milwaukie and North Clackamas County.
"Siemens is proud to be a technology partner for Trimet for more than 30 years, starting in the this project is a perfect example of how advanced rail technologies can help to revitalize city centers, creating jobs and stimulating economic development", said Jochen Eickholt, CEO Siemens Mobility Division.
The newly redesigned light rail vehicles were built based on input from TriMet and riders, featuring new seating arrangements, additional wheelchair accessibility, larger windows and improved HVAC systems that automatically adjust based on the number of people in the vehicle. The vehicles also include better sight lines for the driver, more ergonomically designed main cabins, and larger displays for train operators so they are better able to monitor the vehicle's status to improve safety and efficiency. Maintenance enhancements were made based on TriMet's feedback including rearrangement of systems to increase accessibility to key components on the vehicles and improved diagnostic systems.
The innovative regenerative rail energy storage technology allows for energy created during braking to be stored and then re-used in one of two forms, energy savings or voltage stabilization during peak demand times. TriMet will utilize the system in voltage stabilization mode. In this mode, the storage unit allows the system to avoid problems disruptions that can occur in mass transit operations if power drops below a certain level. If a number of vehicles accelerate simultaneously, system voltage can drop below a critical level and result in instances of under-voltage tripping in vehicles and, consequently, lead to disruptions in passenger service. The Sitras SES ensures the system voltage always remains within the required range and voltage-related disruptions no longer occur.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at www.siemens.com.