Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 July 2017MobilityMunich
Prototype of the Rhine-Ruhr Express presented
"The start of tests at the PCW shows that we're right on schedule with the RRX project. We're testing here whether the trains are fit for their daily service in and between the cities in North Rhine-Westphalia. Each train of the entire RRX fleet will be commissioned right here, virtually on the doorstep of the public rail network," said Sabrina Soussan, CEO of Siemens' business with high-speed and regional trains and locomotives.
Siemens was commissioned in March 2015 by the special-purpose associations Nahverkehr Rheinland (NVR), Nahverkehr Westfalen-Lippe (NWL), Schienenpersonennahverkehr Rheinland-Pfalz Nord (SPNV-Nord), the Verkehrsverbund Rhein-Ruhr (VRR) and the Nordhessischer Verkehrsverbund (NVV) to deliver 82 multiple-unit electric Desiro HC trains and provide their maintenance for a period of 32 years. The order has a total volume of over €1.7 billion.
Siemens has developed a new design for the RRX fleet based on the successful Desiro platform. The train's concept combines premium features with state-of-the-art technology. Each train consists of four cars; the first and last as end car and driving trailer have one passenger deck, while the two middle cars are double-deckers. Each train has a seating capacity of 400. The trains are designed in a white, grey, black and orange color scheme. The design of the RRX continues into the interior, where generous sight lines and large windows provide a pleasant atmosphere. In addition, the RRX has Wi-Fi access and socket outlets throughout the train, folding tables and reading lights in first-class, as well as advanced information systems and energy-efficient traction units and air-conditioning.
The trains not only offer excellent passenger comfort, but optimal availability throughout their lifecycle. Modern data communication provides a continuous dialogue between the trains and their service facility. As part of the predictive maintenance concept, potential technical faults can be rectified before they actually occur. By taking over the lifecycle service and maintenance of the RRX, Siemens guarantees over 99-percent availability for scheduled operation. With a top speed of 160 km/h and a driver assistance system for look-ahead braking and acceleration, the RRX will ensure optimal traffic flows on heavily traveled routes in the Rhine-Ruhr region.
Further information on the Mobility Division is available at: www.siemens.com/mobility
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Ellen Schramke
Siemens AG
Nonnendammallee 101
13629 Berlin
Germany
13629 Berlin
Germany
+49 (30) 386-22370
Eva Haupenthal
Siemens AG
Werner-von-Siemens-Str. 1
80333 Munich
Germany
80333 Munich
Germany
+49 (89) 636-24421