Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens to supply power train for Sabiya power plant in Kuwait

SGT5-4000F gas turbine

The natural gas-fired Sabiya Extension 3 is being built on the existing site of the Sabiya power plant on the Bay of Kuwait in the country's northeast. It can also be operated with fuel oil as a back-up fuel. The multi-shaft combined cycle power plant will provide an electrical capacity of over 900 MW. The power train from Siemens consists of two SGT5-4000F gas turbines, two hydrogen-cooled SGen5-2000H generators, one SST5-5000 steam turbine, and a SGen5-2000H steam turbine generator. Siemens will also deliver the SPPA-T3000 control system and 26 bays of 400-kV/80-kA gas-insulated switchgear with the associated control and protection systems for the power plant's substation. The substation will provide power to the newly developing areas in northern Kuwait. The long-term service agreement covers the power train components including Power Diagnostics and Remote Monitoring, which are part of Siemens' Digital Services portfolio. Support from Siemens' remote monitoring center is available 24/7 and allows specialists to resolve potential issues remotely before they become serious, just as though they were working on-site.
At present there are six F-class gas turbines running in the Sabiya and Az Zour South power plant projects. "This is the fourth power plant order that Siemens has secured in Kuwait in only four years, following the orders for Sabiya Extensions 1 and 2 and Az Zour South," said Jean Claude Nasr, head of Sales for the Middle East & North Africa Region at Siemens Power and Gas. "The solid partnership with our customers and the high reliability of the existing Siemens gas turbines in Kuwait along with our strong maintenance support surely motivated the customer to choose Siemens' offer from among a number of challenging international tenders."
"Alghanim International has had a very strong partnership with Siemens for more than 15 years that has successfully delivered several projects. We value each other's contributions and understanding of the Kuwaiti power sector, and this robust relationship has allowed us to win most of the competitive bids in the country, giving us the honor of constructing more than 40 percent of the installed capacity in Kuwait. We've also provided O&M services to ensure the highest availability of these plants on par with international utility practices and in compliance with the stringent guarantee conditions imposed by the owner, the Ministry of Electricity and Water," said Tarek Eissa, Group President of Alghanim International.
At the beginning of this year Siemens received an additional order in Kuwait to deliver an industrial steam turbine package to transform the Az Zour South 3 open cycle gas turbine power plant into a combined cycle power plant. This plant is also operated by MEW. The expansion will increase the total installed capacity of the plant by 263 MW without using any additional gas.

For further information on SGT5-4000F, please see www.siemens.com/sgt5-4000f
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet www.siemens.com.
Read more
Reference Number: PR2017070355PGEN

Contact

Susanne Weissmann

Siemens AG

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 18-85753