Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Modular components for networked air handling units

The picture shows the Climatix C600 controller.

At the heart of the new modular system are Climatix C600 controllers capable of reliably controlling even complex applications. They are equipped with faster processors and more application storage and are able to communicate through any of the standards commonly used in building technology. Using the Climatix IC cloud solution, they offer secure remote access to the connected system and ensure high system performance and efficient remote maintenance based on user-specific cockpit information.
Other components of the system include Modbus-capable damper and valve actuators as well as sensors. Thanks to the controllers' expanded connectivity, integrating the new communicating actuators and sensors into air handling units (AHUs) is extremely cost-efficient. The bus topology simplifies the AHU wiring concept, reducing material and labor costs in production up to 30 percent. The wiring effort, and hence the error rate, decrease significantly. In addition, any valve and air damper actuators connected to the Climatix controllers are automatically integrated into the controller application.

For further information on the Building Technologies Division, please see www.siemens.com/buildingtechnologies
For further information on Climatix and OEM solutions from Building Technologies, please see www.siemens.com/buildingtechnologies-oem
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Marc von Ah

Siemens AG

Gubelstrasse 22
CH-6301 Zug
Switzerland

+41 (41) 724-5617