Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release29 November 2017Process Industries and DrivesNuremberg
Simit V9.1 - simulation for faster commissioning and operator training

Simit enables real-time simulation and emulation for the comprehensive evaluation of automation solutions. Testing and optimization can be carried out either using a real or a virtual automation system, the so-called virtual controller. Connection to Comos enables an end-to-end data flow between engineering and simulation, and provides the basis for creating a plant's digital twin.
For improved convenience, in the current version 9.1 the Simit Unit Administration has now been integrated into the Simit user interface. Another benefit for users: A mouse click is all it takes to change quickly and easily between software- and hardware-in-the-loop at any time. Configuration of PLCSIM Advanced coupling has also been simplified. The data required for interface configuration is imported from the engineering data of existing Simatic projects. Using PLCSIM Advanced, virtual controllers can be generated to simulate Simatic S7-1500 and ET 200SP controllers and used to perform extensive function simulation.
Simit offers various automatic modeling functions for simple, rapid simulation modeling. Simulation models and components can be automatically generated, for instance with the aid of template-based imported data. As a result of automatic modeling, practically fault-free simulations can quickly be generated. At the same time, the models and components are automatically parameterized, substantially reducing the outlay of time and costs. A new feature of Simit 9.1 is the ability to perform bulk engineering using spreadsheet calculation. Depending on the selected hierarchy level, it is possible to export the data to Excel. The Simit import wizard enables automatic simulation modeling based on the respective templates.
The new Chem Basic Library is another new addition to Simit. It enables a rapid entry into project engineering using Simit by making available component types to the user, in particular for the simulation of pipeline networks in the chemical and pharmaceutical industry.
Simit Simulation Platform supports different communication interfaces and standards for extended data exchange between simulation and automation environments. Simit can use these to interact with other software applications or programs such as simulation software, or to exchange data with hardware controllers from different manufacturers. Version 9.1 of Simit now also supports the open communication standard OPC UA Client.
To improve efficiency, openness and flexibility, Simit 9.1 supports the current Simatic PCS 7 V9.0, Route Control for engineering, control and diagnostics of material transport, and Safety Matrix, the management tool for every phase of the safety lifecycle. The virtual controller now also simulates the new CPU 410E, the entry CPU for small applications.
The Simit Unit also supports the distributed I/O system Simatic ET 200SP HA, Simatic Compact Field Unit (CFU), R1 Redundancy and PROFINET Process Alarm. Simit Unit documentation is available in XML format and can be simply and rapidly imported from 3rd party engineering tools. From Version Simit 9.1 onwards, Windows Server 2016 is also supported.
More information is available at www.siemens.com/simit
More information on Siemens at the SPS IPC Drives is available at www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017110078PDEN
Contact
Evelyne Kadel
Siemens AG
Klaus-Bungert-Str. 6
40468 Dusseldorf
Germany
40468 Dusseldorf
Germany
+49 (211) 6916-1003