Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 March 2017,
updated20 March 2017Digital Factory Nuremberg
Basic industrial PCs for many different applications in the price-sensitive segment

The picture shows the new Simatic IPC portfolio.
With the new Simatic IPC327E and IPC377E Basic IPCs, applications can be implemented quickly if they do not have specific requirements with regard to certificates, higher temperature ranges or protection classes in the industrial environment. As with all Simatic IPCs, the quality and design of the devices make them suitable for industrial applications, with the selection and harmonization of the individual components and the fanless design with a sealed enclosure offering robustness and a long service life. The state-of-the-art PC technology and multitude of interfaces mean that they can be easily integrated into new and existing automation solutions. They come equipped with an Intel Celeron quad-core processor, a 500 gigabyte hard drive, a VGA and DisplayPort, a PCIe mini-interface, two Gigabit Ethernet interfaces, and up to six COM and USB 3.0 interfaces.
Background information:
The new Simatic IPC327E Box PC and the Simatic IPC377E Panel PC from the Basic IPC series are part of the portfolio of Simatic Industrial PCs from Siemens. This includes the scalable Box, Panel and Rack PC product lines in the performance classes Basic, Advanced, High-End and Embedded, supplemented by additional versions for special applications. The Simatic IPC range – from the compact fanless embedded device to the powerful, expandable high-end IPC – is specifically designed for industrial applications. For mobile automation engineering, users also employ the Simatic Field PG industrial programming device and the Simatic Industrial Tablet PC for mobile automation tasks.
Further Information about the Basic PC at www.siemens.com/ipc327E
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017030177DFEN
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945