Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release11 April 2017Process Industries and DrivesNuremberg
New Logo!Power supply devices for up to 100 watts in ultra-narrow design

the 4th generation of Logo!Power
The integrated current monitor provides a new level of convenience during commissioning and servicing. The current output is read out in real-time as a voltage value using a measuring point. Simple measurement using a voltmeter means that the disconnection of cables by the user for conventional current measurement is no longer required, and the system continues to be supplied with direct voltage without interruption. Users also benefit from a new downward extended operating temperature range of -25° to +70° Celsius, and scope for worldwide application with a wide range of certifications.
The innovated Logo!Power series with its housing widths of 18 to 72 millimeters is the compact successor to the previous 3rd generation. The new variants with 24 V/0.6 A and 12 V/0.9 A extend the portfolio for very small outputs and come in a width of just one 18 mm pitch. A total of eleven devices with regulated and adjustable output voltages of five, twelve, 15 and 24 volts (V) supply an output of up to 100 W. Their wide-range input allows these power supply devices to be operated at all single-phase supply networks with 110 to 240 V AC nominal voltage and even at direct voltage networks with 110 to 300 V DC without the need to switch over. For capacitive loads on power supply start-up, a power reserve of 150 percent is available, and the constant current behavior compensates for overloads during operation. A diagnostic LED signal "DC O.K." indicates the status of the power supply device. Fields of application for Logo!Power in industrial automation include simple packaging machines, garbage presses, conveyor belts, sorting systems, infeed units and sterilizers. In the field of building technology, the power supply devices can be used for lighting controls, such as panic circuits, central and random circuits, heating control system extensions, door and gate controls, and access restriction. Logo!Power devices are also found in pumping stations, special-purpose vehicles, saunas, swimming pools and automatic livestock feeding devices.
For further information on Logo!Power, please see www.siemens.com/logo-power
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017040161PDEN