Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens opens grid control center of the future with research and scientific partners

The picture shows the grid control center at the Technical University of Ilmenau, Germany.

"A priority objective was to develop what we might call an autopilot for the transmission network. Like an aircraft, the autopilot has two core functions: first, to control the system automatically so that the "flight" or grid operation remains as calm and stable as possible at all times. Its second function is to detect obstacles or faults at an early stage so that they can be circumvented or avoided. This allows the operator in the dynamic grid center to identify the dynamic conditions in the grid. What we'll do is provide the operator with the means to react effectively to verified dynamic grid conditions, something that's not possible today," said Prof. Dr. Rainer Krebs, principal expert and head of the Technical Department for Protection and Control System Studies in the Siemens Energy Management Division.
The research consortium consists of Siemens, the universities of Magdeburg, Ilmenau, and Bochum, and the Fraunhofer Institutes in Magdeburg and Ilmenau. The dynamic grid center will be the answer to the growing problem of controlling dynamic conditions in the transmission grid. Grid requirements have already changed enormously: Large nuclear power plants and coal-fired power plants are being taken off the grid, and the new focal points for power generation are the large-scale wind farms in the North Sea. In addition, a distributed and fluctuating power supply is fed in at all voltage levels from wind turbines and countless photovoltaic systems across all of Germany.
In order to ensure that the electrical power is delivered where it's needed without detours – even under the aggravated conditions of increasingly dynamic grids, longer transmission paths, and less-than-precise forecasting for renewable energy sources – the experts have developed the dynamic grid control center, and a prototype has been installed in Ilmenau. The planned high-voltage DC transmission routes in the three-phase grid are also included. They will help stabilize the grid if the control algorithms of a smart HVDC transmission control system are integrated in the operation of a dynamic grid control center. Complex energy systems are being modeled in a real-time simulation being conducted in Ilmenau, and the kinds of operating conditions that are expected in the future are being analyzed. The accumulated data must be processed such that a single person can collect this data and can act immediately, if necessary. Although there's already a high level of automation in grid control centers today, responsibility for decision-making still lies with the control center personnel.
This essentially visual processing of data also poses a challenge, because the dynamic grid control centers no longer simply receive and analyze conventional measured values. Another concern in the future will be the integration of synchronized, high-precision measurement equipment that can measure phase angle as well as voltage, current, and frequency. This not only means that there is a significantly more accurate and dynamic grid model available in milliseconds; there are also far more precise recommendations for action that will be made to the control center personnel. Today control centers already have to intervene in the grid with increasing frequency to keep voltages, currents, and grid frequency within the permissible limits. The work in progress in Magdeburg and Ilmenau could very soon result in dynamic control centers replacing conventional control centers in the grid as a long-term solution to the problem of increasing grid dynamics.
The three-year-long DynaGridCenter research project was kicked off at the Otto-von-Guericke University Magdeburg in October 2015. The project partners are Siemens, the Otto-von-Guericke University Magdeburg, Ilmenau Technical University, the Ruhr University Bochum, the Fraunhofer Institute for Factory Operation and Automation (IFF) in Magdeburg, and the Fraunhofer Institute of Optronics, System Technologies, and Image Exploitation, Advanced System Technology branch (IOSB-AST) in Ilmenau. Associated project partners are the transmission grid operators 50Hertz Transmission, TransnetBW, TenneT, and Amprion. Siemens is responsible for coordinating the joint project, which has received roughly €5 million in funding from the German Federal Ministry for Economic Affairs and Energy. The project will cost a total of €7.2 million.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2017030216EMEN

Contact

Dietrich Biester

Siemens AG

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 7-33559