Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

New servo drive system simplifies project engineering for machine builders

The picture shows the Sinamics S210 converter and the newly developed Simotics S-1FK2 motor from Siemens.

The functional scope of the Sinamics S210 focuses on highly dynamic motor axis control, while the connected controller, for instance the Simatic S7-1500 or S7-1500T with its extended motion control functionality, takes complete charge of positioning functions for the connected drive axes. The converter is commissioned entirely using an integrated web server. The one-button tuning function allows automatic optimization of control parameters, taking into consideration the behavior of the connected mechanics by different dynamic levels. The integrated safety functions include STO (Safe Torque Off) and SS1 (Safe Stop 1). Both can be actuated using PROFIsafe, STO additionally using a terminal. Additional functions are currently in the preparation stage. In conjunction with the rapid sampling and smart control algorithms of the Sinamics S210, a high-grade encoder system and the combination of low rotor inertia and high overload capability, the servo motors achieve outstanding dynamic performance and precision. Siemens will be showcasing the relevant motors in shaft heights of 20, 30 and 40 millimeters at the Hannover Messe at the end of April 2017.
By using the Motion-Connect OCC to connect the Simotics S-1FK2 motors to the converters, the power conductors, encoder signal and brake are grouped together in an exceptionally thin cable measuring just 9 millimeters in diameter, and use a single plug. Its minimal cross-section makes the OCC cable thinner, lighter and more flexible than previous power cables, considerably simplifying the cabling process. For drag chain applications, there is also a compact one cable connection available which reduces the bending radius to almost half compared to conventional drag chain conductors. The connecting plug comes in a rugged design despite being rotatable and easy to operate at a height of 25 millimeters. Cabling at the converter is just as simple with benefit of user-friendly self-locking plugs and easy-access detachable push-in terminals on the front.

For further information on drive system Sinamics S210, please see www.siemens.com/sinamics-s210
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Guenter Gaugler

Siemens AG

Wittelsbacherplatz 2
80333 Munich
Germany

+49 (89) 636-34782