Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

New switch disconnectors with Sitor fuses for semiconductor protection

Switch disconnectors with Sitor fuses

3KF switch disconnectors with fuses fulfill all requirements of a main switch, emergency stop or repair switch. In case of system malfunctions, they protect the operating personnel from electrical accidents and can be used in floor distributions for network disconnection. Padlocks for front or side wall operating mechanisms protect against unauthorized switching. Terminal covers prevent direct contact with live components. Plug-on phase barriers protect against arcing. Optimal fuse monitoring indicates tripped fuses for an immediate response.
The 3KF switch disconnectors with Sitor fuses (LV HRC design) are suitable for AC applications up to 690 volts and DC applications up to 440 volts. Siemens offers the switch disconnectors in five sizes for applications of 32 amps (A) up to 800 amps, all of which are available in three- and four-pole designs. The units can be easily installed, and additional functions can be retrofitted at any time. The switch disconnectors can be attached to mounting plate or by snapping them onto standard mounting rails. Connection is made through box terminals or flat connections. The integrated test function verifies the correct cabling of the control circuits.

For more information about the Energy Management Division please visit www.siemens.com/energy-management
For more information about switch disconnectors please visit www.siemens.com/switching-devices
More information about the Light+Building can be found at:
www.siemens.com/press/lightbuilding-2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Heidi Fleissner

Siemens AG

Siemensstr. 10
93055 Regensburg
Germany

+49 (941) 790-2212