[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release22 November 2017Digital Factory Nuremberg
All-round IP65-protected Panel and Panel PC for user-friendly operator control and monitoring
New, all-round IP65-protected Panel and Panel PC for machine-related, cabinet-free visualization and automation
Simatic HMI TP1200 Comfort Panel PRO and Simatic IPC477E PRO Panel PC: high performance and functionality, many interfaces
Used in high-end applications and for high-performance visualization tasks
Extended individual operation through extension units: standard components for tailor-made system solutions
Siemens has extended its system family based on IP65-protected HMI (Human Machine Interface) devices for machine-related, cabinet-free visualization and automation. The Simatic HMI TP1200 Comfort Panel PRO (PROtected) with 12-inch display diagonal and the Simatic IPC477E PRO industrial Panel PC with 15, 19 and 22-inch displays are characterized by high performance and functionality as well as a large number of integrated interfaces. The new operator control and monitoring devices are especially suitable for high-end applications and powerful visualization tasks. Flexible mounting types allow the user easy operation of the machine and an optimal view of the visualization and process.
New, all-round IP65-protected Panel and Panel PC for machine-related, cabinet-free visualization and automation
Simatic HMI TP1200 Comfort Panel PRO and Simatic IPC477E PRO Panel PC: high performance and functionality, many interfaces
Used in high-end applications and for high-performance visualization tasks
Extended individual operation through extension units: standard components for tailor-made system solutions
Siemens has extended its system family based on IP65-protected HMI (Human Machine Interface) devices for machine-related, cabinet-free visualization and automation. The Simatic HMI TP1200 Comfort Panel PRO (PROtected) with 12-inch display diagonal and the Simatic IPC477E PRO industrial Panel PC with 15, 19 and 22-inch displays are characterized by high performance and functionality as well as a large number of integrated interfaces. The new operator control and monitoring devices are especially suitable for high-end applications and powerful visualization tasks. Flexible mounting types allow the user easy operation of the machine and an optimal view of the visualization and process.
The picture shows the Simatic HMI TP1200 Comfort Panel PRO with 12-inch display diagonal.
For powerful, PC-based HMI applications, the technology of the improved E generation of industrial Panel PCs is installed in the Simatic IPC477E PRO Panel PC – with 6th generation Intel Core i processor and modern Celeron and Xeon processors. The new Panel PC has a wide range of interfaces, such as 3x Gigabit Ethernet, 4x USB 3.0 and optional 2x COM to facilitate flexible use. Extension units –mountable components – extend the operation of the all-round IP65-protected PRO devices. The 12 to 22-inch extension units, which consist of standard components such as basic device, extension components, mounting adapters, keyboard tray and an optional keyboard also available in IP65 stainless steel versions, allow tailor-made system solutions. They are characterized by easy mounting and commissioning, as well as user-friendly engineering, and can be easily adapted to meet individual customer requests. A large selection of control elements is also available: from indicator lights, selector and key switches, Emergency OFF mushroom pushbuttons, USB interface and RFID reader, all the way to a stainless-steel keyboard. The control elements are easily and quickly labeled with label holders and inscription plates, or inscription plates and lens assemblies. The extension unit is now also available in a fail-safe Profisafe version, in addition to the conventionally hard-wired and bus-capable Profinet version.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.