[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release02 November 2017Process Industries and DrivesNuremberg
Enhanced ultrasonic flow system with high accuracy and low cost of ownership
New, low-cost Sitrans FS220 clamp-on ultrasonic flow system
User-friendly interface with setup wizards for simplified operation
High accuracy of 1% of flow rate
Newest addition to portfolio of next-generation digital flow systems
Siemens launched the Sitrans FS220 clamp-on ultrasonic flowmeter, the newest addition to the growing portfolio of next-generation digital flow measurement systems from Siemens. Combining the Sitrans FST020 transmitter with Sitrans FSS200 externally mounted sensors, the Sitrans FS220 offers the most commonly required measurement functions with superior accuracy, cost efficiency and ease of use. The new flow system is suitable for multiple industries requiring budget-conscious liquid flow instrumentation, including water and wastewater, power, HVAC and chemical.
New, low-cost Sitrans FS220 clamp-on ultrasonic flow system
User-friendly interface with setup wizards for simplified operation
High accuracy of 1% of flow rate
Newest addition to portfolio of next-generation digital flow systems
Siemens launched the Sitrans FS220 clamp-on ultrasonic flowmeter, the newest addition to the growing portfolio of next-generation digital flow measurement systems from Siemens. Combining the Sitrans FST020 transmitter with Sitrans FSS200 externally mounted sensors, the Sitrans FS220 offers the most commonly required measurement functions with superior accuracy, cost efficiency and ease of use. The new flow system is suitable for multiple industries requiring budget-conscious liquid flow instrumentation, including water and wastewater, power, HVAC and chemical.
The picture shows the Sitrans FS220 clamp-on ultrasonic flowmeter
The new Sitrans FST020 transmitter with its integrated PerformancePLUSTM algorithm has been upgraded from the previous version to deliver enhanced performance, simplicity and options for customization. It measures with consistently high accuracy of 1% of flow rate, improved zero stability resulting in minimal need to set a zero point and repeatability of 0.25% according to ISO 11631.
The Sitrans FST020 provides a user-friendly experience from initial startup through day-to-day operation and servicing. The large graphical display features intuitive menu navigation, multiple setup wizards, and the ability to display up to 6 user-configurable parameters on the same screen as well as to customize 5 different views. The innovative SensorFlash® microSD card provides access to all product data and certificates directly from a PC or via the transmitter's built-in USB service port. Its datalogging and audit trail feature automatically stores up to 100 records per log of process and diagnostic parameters or changes made to device settings. This function allows operators to analyze the performance of each process and address any potential issues, resulting in optimized plant efficiency and higher-quality end products. And the transmitter's digital platform is proven in use, as it shares HMIs and menu structures with the more advanced FST030 clamp-on ultrasonic transmitter as well as the FCT030 Coriolis transmitter.
The Sitrans FST020 transmitter has been developed to work with the existing line of Sitrans FSS200 clamp-on ultrasonic sensors, which can be installed on pipes as large as 10 m (394 in) with no process downtime. As the sensors never make contact with the medium and do not feature any moving parts, they require virtually no maintenance. Additionally, for the most challenging applications, optional WideBeam® transit-time sensor technology handles high levels of aeration or suspended solids without any significant reduction in performance.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.