Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Simplified handling of Sinamics V-converters with new frame size and Profinet connectivity

The picture shows the SINAMICS V20 Basic converter from Siemens.

The picture shows the SINAMICS V90 Basic Servo Drive System from Siemens.

The Sinamics V20 from the Siemens portfolio is a basic converter which benefits from exceptionally short commissioning times, cost efficiency, simple handling and a robust design. The standard converter is available in nine frame sizes.
There have also been some innovations in the Sinamics V90 servo drive portfolio, where the smallest frame size FSA is now also available as a Profinet version for 0.1 and 0.2 kW, which are covered by frame size FSB at the moment. These changes have enabled the footprint to be reduced by 10 millimeters, making the V90 FSA frame 18 % smaller. It is now also possible to transmit process and diagnostic data over the Profinet interface in real time using a single cable.
Within the V90 servo drive system the Simotics S-1FL6 (SH45, SH 65 and SH90) motor series has also been released in a more compact design, with the connections now angular on the motor side, but straight on the cable side. The Sinamics V90 servo drive system is particularly suited for highly dynamic applications.

For further information on Sinamics V20, please see www.siemens.com/sinamics-V20
For further information on Sinamics V90, please see www.siemens.com/sinamics-V90
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2018030204DFEN

Contact

Katharina Lamsa

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7975