Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release06 April 2018MobilityMunich
Siemens will digitalize the Norwegian Railway infrastructure
"This marks the start of modernization of the railway network in Norway. Bane NOR is creating the railway of the future with one of Norway's largest digitization projects. We are confident, that Siemens, by winning the contract to provide a new digital signal system, will contribute significantly to our network's modernization," says Sverre Kjenne, Bane NOR Executive Vice President.
"This project is a major step in signaling history - a technology step only comparable to the change from relay to electronic interlockings in the 80s. Together with Bane NOR Siemens will renew the complete Norwegian rail network into a full digital IP based system - a real 'Internet of Things' system. This will save much hardware, allow for maximized capacity and provide the basis for data based minimized preventive maintenance. In the end it will allow to give passengers a far more efficient and reliable travel experience with far higher punctuality, increased capacity and throughput. All will be controlled via a central interlocking in Oslo, which gives the trains the authority to proceed via our ETCS Level 2 solution. The contract is not only the largest single delivery for Siemens in Norway, but also for the Siemens rail infrastructure business ever," says Michael Peter, CEO of the Mobility Division.
The investment in ETCS is a major step in a Norwegian railway revolution. Bane NOR will invest more than 2 billion euros in digitalization and automation of its railway network over a ten-year period. This will be done through Bane NOR's ERTMS (European Rail Traffic Management System) initiative, and will make Norway a pacesetter in using digital technology in the rail sector.
With the new ETCS technology, the Norwegian rail system's signaling system will be digitalized. The project's scope of delivery includes the complete signaling system with interlockings, ETCS Level 2 system, point machines, train detection systems, level crossings and associated infrastructure along the lines. Implementation will be carried out during ongoing operations. The first line to be equipped with the new signaling system will be the Nordlandsbanen and is scheduled to begin operation in 2022. The introduction of ETCS in the Oslo area is planned for 2026. Completion of the new interlocking and train control system is planned by 2034.
The Sinet distributed smart safety system is based on industry standard communication interfaces and includes functionality for cloud-based services. With the ETCS as a cab-signaling system, main signals are no longer required along the lines since signal aspects are directly transferred to the driver's cab. This will make railway operation more efficient.
The system is part of a European standard that will replace today's more than 20 different train management systems. With ETCS train interoperability, routing throughout Europe can be achieved. For example, a freight train can be driven from Italy up to Norway without having to change locomotives at borders. This will make the transportation of goods and passenger both quicker and cheaper than today.
Benefits: ETCS Level 2 not only reduces infrastructure costs to a significant extent, but also increases line capacity and reducing journey times.
This press release and for information are available at: www.siemens.com/press/ERTMS-Norway
For further information about the Mobility Division, please see: www.siemens.com/mobility
For this press release
@SiemensMobility
@SiemensMobility
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Anne-Muriel Alexici
Siemens AG
Otto-Hahn-Ring 6
81739 Munich
Germany
81739 Munich
Germany
+49 (89) 636-24407