Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release17 April 2018Energy ManagementDenver
Siemens black-start technology to provide critical back-up for San Francisco's power grid

The picture shows the Trans Bay Cable HVDC transmission station San Francisco.
This feature, known as black-start capability, will allow up to 300 megawatts (MW) of power to be directly fed into the city through Trans Bay Cable, while the remaining network is being restored. The black-start capability, which does not require the San Francisco local network to be up and running, will provide electricity across the city to power critical infrastructure like hospitals, fire stations, and emergency centers.
"On any given day, TBC can provide about half of San Francisco's power needs, so our ability to provide reliable, consistent electricity is extremely important," said Steven Powell, Trans Bay Cable. "We're happy to have Siemens as a technology partner in this project and with their black-start technology, an upgrade to the system that was completed on-schedule and on-budget, which enables TBC to continue to deliver critical power during an emergency."
"The city of San Francisco and its residents depend heavily on reliable power. That becomes even more of a priority during times of emergency, such as an earthquake or other catastrophic event, when providing power to critical systems is paramount," said Mirko Düsel, CEO Transmission Solutions at Siemens Energy Management. "By routing emergency power directly into the city using Siemens' technology, Trans Bay Cable's new black-start capability will be able to use existing infrastructure to provide emergency power during a challenging time."
Siemens' modular multi-level (MMC) converter is the world's first to be successfully tested for black-start capability using load banks. The new functionality is an extension of the company's existing partnership with Trans Bay Cable, which currently utilizes Siemens' HVDC converter station systems to transmit power via submarine cable which traverses the San Francisco Bay from a converter in the East Bay to the Potrero converter station in the heart of San Francisco. The submarine cable system has helped relieve congestion and provides transmission reliability for the Bay Area, while obviating the need to site and build additional generation in a dense population center.
The commissioning and testing of the upgraded project control system included highly-specialized load banks from ComRent and installation by Cupertino Electric, Inc.
For further information on HVDC, please see https://www.energy.siemens.com/hq/en/power-transmission/hvdc
For this press release
Links
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2018040157EMEN
Contact
Sabrina Martin
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-37168