Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release23 April 2018Digital Factory Hanover
Industrial Edge from Siemens adds benefits from the cloud at the field level
Infographic: Siemens Industrial Edge
With Siemens Industrial Edge, Siemens is offering users the chance to close the gap between classic, local data processing and cloud-based data processing to suit individual requirements. Edge Computing allows large volumes of data to be processed locally. To this end, Siemens is releasing a broad spectrum of applications to users, including data processing, data visualization via webservers, data transfer to the cloud or IT infrastructures, and quick innovation cycles in the development of apps. There is also an additional reduction in memory and transfer costs as large volumes of data are preprocessed and only the relevant data is finally transferred to a cloud or IT infrastructure. Siemens Industrial Edge supports cloud transfer protocols for MindSphere, Siemens' own open, cloud-based operating system. In the future, it will also support Message Queuing Telemetry Transport (MQTT), making data transfer safe, secure and effective.
Stable processes and increased productivity for machine tools
Industrial Edge with Sinumerik provides a machine-level platform for software applications which captures, preprocesses and analyzes high-frequency data. In addition to this, calculations can be carried out for complex machine tools and auxiliary process times or workplace monitoring can also be optimized. Both operating system and application in Industrial Edge for Sinumerik are installed and continuously kept up to date via backend services on MindSphere, the open, cloud-based IoT operating system from Siemens. Industrial Edge for Sinumerik thus provides users with continuously stable process and condition monitoring as well as significantly higher productivity.
Extremely high flexibility and productivity for manufacturing plants throughout the whole life cycle
Siemens is offering users a platform for implementing today's demands and those of the future in the form of Industrial Edge with Simatic. Automation components such as Simatic controller are provided with supplementary support through Edge Devices in order to process greater volumes of plant data profitably and to gain information for a continuous increase in productivity. At the same time, new applications such as condition monitoring or predictive maintenance are being introduced into classic automation technology. In addition to this, Edge Computing also provides access to previously unknown degrees of flexibility, allowing plants to be kept right up to date via functional, feedback-free updates - and all within standard plant life cycles for automation. Siemens apps development supports users with frameworks and access to integrated connectivity to the world of automation.
Siemens Industrial Edge includes Edge Management, Edge Devices and Edge Apps
Siemens Industrial Edge includes Edge Management, Edge Devices and Edge Apps. The Edge Management System provides central control of all connected Edge Devices as well as condition monitoring. Users can use the Edge Management System to install software applications (Edge Apps) onto the required Edge Devices from the Edge App store in the backend system, e.g., MindSphere. Edge Devices are equipped with an Edge runtime software which guarantees the connectivity for both data capture from the connected automation element and for Edge Management: It also has a driver toolbox for access to device functions. The Edge runtime software also provides a secure app environment for executing functions on Edge Devices. Edge Apps for Siemens Industrial Edge are available from Siemens as well as third-party providers. In addition, it will also be possible for users to develop their own Edge Apps tailored to individual requirements.
For further information on the topic of Siemens Industrial Edge, please see www.siemens.com/industrial-edge
For this press release
Event: Siemens at the Hannover Messe 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975