[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release03 December 2018Process Industries and DrivesNuremberg
Cost-effective, compact level transmitter with intelligent processing for improved accuracy
Improved accuracy and repeatability
Increased asset utilization and decreased operational waste
Wide range of applications in environmental, chemical, and food and beverage industries
Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
Improved accuracy and repeatability
Increased asset utilization and decreased operational waste
Wide range of applications in environmental, chemical, and food and beverage industries
Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
The picture shows the Sitrans Probe LU240
Sitrans Probe LU240's four-button user interface or remote configuration with Simatic PDM ensures fast and easy setup. Operators will save time and maintenance costs with Sitrans Probe LU240's transparent lid: in manual observations, users can observe values directly instead of by removing the device's lid. For those applications requiring process temperature data, Sitrans Probe LU240 now gives users both level and temperature readings. The device is also battery and solar-power friendly due to a low start-up current of 3.55 mA and minimum 10.5-volt operation.
In dirty applications or those with buildup, the transmitter's maintenance-free active face technology keeps the sensor clean and is also unaffected by wind, rain, snow or temperature changes. And for rugged applications in harsh environments, it is IP68 fully potted and encapsulated with a PVDF sensor resistant to corrosion, chemicals, and extreme shock.
Digitalization integrates critical field data into a plant's entire operations, unlocking new opportunities to analyze processes and identify areas for improvement. By connecting Sitrans Probe LU240 to a control system, operators can monitor level measurements from the comfort of the control room or on the go using a solution from the suit of Siemens automation or remote products.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet www.siemens.com.