Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 February 2019Digital Factory Nuremberg
Siemens presents solutions for the digital transformation of the intralogistics sector
Digital Enterprise portfolio for intralogistics
The Plant Simulation and Process Simulate software allow operators and machine builders to optimize individual machine components right through to complete lines. Various solution scenarios can be simulated, visualized, and analyzed in advance allowing the demands on new systems to be defined, and potential bottlenecks to be identified. Machine builders can produce entire digital mechatronic concepts using NX Mechatronic Concept Designer – from mechanics, via electrics, to automation. Automation Designer is available to create an integrated engineering solution for the electrical and automation systems in digital plants. By automatically generating PLC code for the TIA Portal and transferring this into PLCSim Advanced, the S7 controller can be put into virtual operation which significantly reduces the cost of the subsequent physical commissioning. The use of MindSphere applications during operation allows cloud-based solutions such as the innovative service concepts to be implemented, increasing the productivity and availability of machines and systems. The performance of intralogistics systems and their automation and drive components can be analyzed using the open, cloud-based IoT operating system, MindSphere. All the information gained can be fed back to the overarching value chain for continuous optimization.
Highlights: AGVs, localization systems, sorting solutions, storage and retrieval machine concepts
Siemens will be using an automatic guided vehicle (AGV), a storage and retrieval machine, and a localization system with Simatic RTLS to illustrate how the Digital Enterprise Suite can be used in intralogistics tasks. Using Simove, the AGV system platform, Siemens will be demonstrating how AGV machine builders benefit from reduced planning and engineering effort as well as shorter commissioning times, and how users can design their logistics processes more flexibly and productively. The Simove offer includes maintenance applications as well as fleet management software which forms an integration platform for AGVs from different manufacturers. The Simove software library contains a range of pre-configured and tested functional modules for machine builders. The Simove software is also based on the Simatic TIA Portal which facilitates efficient engineering.
Siemens will also be demonstrating how the Simatic RTLS (Real Time Location System) can be used to optimize logistics processes, navigate material flows, and control mobile robots. The localization platform produces real-time data on the location and status, supplying intelligent data on location, movement and status. This supports holistic use of the logistics processes and resources in terms of quality, costs, and flexibility.
At Logimat, Siemens will be presenting an integrated solutions portfolio for sorting solutions, comprising hardware and software. The focus is on processing particularly small packages in a range of sizes and weight groups. Siemens will be showing how VarioRoute quickly splits streams of packages and how the software-based address reader IDEW optimizes manual sorting.
At Logimat, Siemens will be presenting an integrated solutions portfolio for sorting solutions, comprising hardware and software. The focus is on processing particularly small packages in a range of sizes and weight groups. Siemens will be showing how VarioRoute quickly splits streams of packages and how the software-based address reader IDEW optimizes manual sorting.
In addition to this, Siemens will be demonstrating solution concepts for storage and retrieval machines at Logimat which can cope with the high demands on flexibility, speed, and accuracy. Anti-sway solutions, energy-efficient drives with the Sinamics S120 frequency converter, and features such as speed synchronization and load distribution will also be on display and Siemens will demonstrate the new version (3.0) of the TÜV-certified safety library which has been specially developed for storage and retrieval machines. Benefits to users from the safety library V3.0 include quicker commissioning which can include fail-safe Simatic controllers (from S7-1516F).
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975