Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Expanding the flagship fleet: Deutsche Bahn orders additional ICE 4 Trains

“The ICE 4 is our absolute pride and joy. This new order shows that the power car principle we developed – a complete novelty in high-speed transport – offers Deutsche Bahn exactly the flexibility it needs to quickly respond to changing transport requirements. We can thus guarantee DB sustainable value development over the train’s entire lifecycle,” said Sabrina Soussan, CEO of Siemens Mobility.
The ICE 4 was designed as a trainset with the greatest possible adaptability. Twenty-four different trainset configurations can be ordered on the basis of five car types. The prerequisite for this freely configurable design is the power car that has all key traction components and traction power units located beneath the floor. The trainsets can be configured with power cars, a service car, middle cars and two end cars, as well as a restaurant car. A 12-car ICE 4 is driven by six power cars and a 13-car train by seven power cars, and can reach a top speed of 250 km/h. The option of increasing the top speed from 250 to 265 km/h is being considered. This design concept enables DB to flexibly adapt its trains to meet varying needs for passenger capacity and route topography.
All in all, DB will now be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets. DB will keep the remaining two end cars in reserve. The ICE 4 train extended by one car has a length of around 374 meters and a total of 918 seats, 88 seats more than in the 12-car version. In the extended configuration, there are 205 seats in first class, 713 in second class and 22 in the restaurant car. The 12-car and 13-car trainsets will be operated in Germany, Austria and Switzerland. The shorter 7-car trains are planned for use in Germany
and Austria.

For this press release

Feature: Largest order: Siemens is building ICE 4 trains for Deutsche Bahn

Feature: Largest order: Siemens is building ICE 4 trains for Deutsche Bahn

@SiemensMobility

@SiemensMobility

@SiemensMobility

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2017, which ended on September 30, 2017, the former Siemens Mobility Division posted revenue of €8.1billion and had around 28,400 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more
Reference Number: PR2018100015MOEN

Contact

Ellen Schramke

Nonnendammallee 101
13629 Berlin
Germany

+49 (30) 386-22370