Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 May 2019Digital IndustriesHanover
Efficient and digitally networked woodworking – Siemens at the Ligna 2019

Innovative woodworking control system
There is great potential for cutting costs and increasing efficiency in the woodworking and wood processing industry, especially in the control and automation of the individual value-adding processes. The new, open Sinumerik MC CNC is exhibited on a machining center. This control is especially suitable for wood, glass and stone cutting machines, and special technologies in the machine tool industry. The latest generation of the proven Sinumerik NC kernel ensures optimum motion control for woodworking machines. At the same time, the automation performance is improved by the integrated Simatic S7-1500 fail-safe controller. Thanks to the Windows 10 operating system, machine manufacturers can even integrate customized software for controlling and operating woodworking machines. The integration of its own user interfaces and the extensive range of interfaces make the Sinumerik MC a universal, open control system which can be easily integrated into existing machine solutions. Another new feature is engineering through the TIA Portal which simplifies engineering processes and reduces the likelihood of errors, leading to a cut in commissioning times.
There is great potential for cutting costs and increasing efficiency in the woodworking and wood processing industry, especially in the control and automation of the individual value-adding processes. The new, open Sinumerik MC CNC is exhibited on a machining center. This control is especially suitable for wood, glass and stone cutting machines, and special technologies in the machine tool industry. The latest generation of the proven Sinumerik NC kernel ensures optimum motion control for woodworking machines. At the same time, the automation performance is improved by the integrated Simatic S7-1500 fail-safe controller. Thanks to the Windows 10 operating system, machine manufacturers can even integrate customized software for controlling and operating woodworking machines. The integration of its own user interfaces and the extensive range of interfaces make the Sinumerik MC a universal, open control system which can be easily integrated into existing machine solutions. Another new feature is engineering through the TIA Portal which simplifies engineering processes and reduces the likelihood of errors, leading to a cut in commissioning times.
Digitalization boosts productivity and flexibility
The Siemens trade show focuses on the benefits of digitalization which enable companies in the woodworking and wood processing industry to respond quickly to changing customer requirements and the increasing customization of products.
The Siemens trade show focuses on the benefits of digitalization which enable companies in the woodworking and wood processing industry to respond quickly to changing customer requirements and the increasing customization of products.
Siemens is exhibiting a digital twin of a tool changer on the booth. It demonstrates how a project can already be imaged as an exact virtual model in advance of its implementation. This allows the user to simulate the behavior of the workpiece and the machine, optimize performance, and apply the knowledge gained from previous design and production activities. As a result, the ever growing demands on productivity and flexibility can be met. The basis for this is to link the real and virtual worlds, for example through the MindSphere cloud-based, open IoT operating system, which helps machine manufacturers to analyze their machines during operations, and thus draw conclusions for the continuous optimization of processes.
Siemens is also exhibiting new HMI Comfort Panels, the Simatic IPC527G industrial PC, and the high-performance Sinamics S210 servo drive system coupled with Simotics S-1FK2 motors, in the current 400 V versions for a higher performance range up to seven kilowatts.
Further information about Siemens at the Ligna 2019 is available at http://www.siemens.com/ligna
Siemens is also exhibiting new HMI Comfort Panels, the Simatic IPC527G industrial PC, and the high-performance Sinamics S210 servo drive system coupled with Simotics S-1FK2 motors, in the current 400 V versions for a higher performance range up to seven kilowatts.
Further information about Siemens at the Ligna 2019 is available at http://www.siemens.com/ligna
For this press release
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2019050270DIEN
Contact
Julia Kauppert
Siemens AG
Gleiwitzer Str. 555
90475 Nürnberg
90475 Nürnberg
+49 (911) 895-7958