Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Siemens and Netze BW make distribution grids more sustainable and smarter
The innovative substation, which will connect the medium-voltage distribution grid and the low-voltage local grid in the town of Kreuzthal in the Oberallgäu region, is now being tested under real-life conditions
As the largest grid operator for power, gas and water in the EnBW group, Netze BW has 83 locations across Baden-Württemberg, Germany, covering an area of approximately 17,700 km².
www.siemens.com/smartinfrastructure
The core of the station is a blue GIS 24 kV Ring Main Unit (RMU). It combines the Clean Air insulation medium, a mixture of natural, atmospheric gases, with proven and reliable vacuum switching technology.
For this press release
Contact
Anna Korb
Smart Infrastructure
91058 Erlangen
Germany
+49 9131 173 663 7