-
Next milestone in the “H2goesRail” project
- Siemens CEO Roland Busch, DB CEO Richard Lutz and
State Secretary Hartmut Höppner take first test ride in the Mireo Plus H and test
the refueling process
- Innovative complete hydrogen system will be used in regular passenger service
as of 2024 and replace diesel trainset
- Hydrogen train and mobile fueling
station can be viewed at the InnoTrans2022
(Wegberg-Wildenrath,
September 9, 2022) Premiere ride in the new hydrogen train: Dr. Roland
Busch, CEO of Siemens AG, Dr. Richard Lutz, CEO of Deutsche Bahn, and Hartmut
Höppner, State Secretary in the Federal Ministry for Digital and Transport (BMDV),
are taking their first ride in the Mireo Plus H hydrogen train today and will
then demonstrate the train’s refueling procedure using the mobile hydrogen
fueling station. The event will be held at the Siemens Test and Validation
Center in Wegberg-Wildenrath, North Rhine-Westphalia. It is planned to have
hydrogen technology replace diesel-powered trainsets in regional transport in
the future and make a significant contribution to phasing out diesel fuel. Hydrogen
trains are a particularly climate-friendly drive technology since they operate
emission-free with green hydrogen and emit only water vapor.
Deutsche Bahn
(DB) and Siemens Mobility are driving forward the climate-friendly transition
in transport and are testing the use of hydrogen for rail for the first time.
The aim is to test a completely new overall system consisting of a newly
developed train and a newly designed filling station.
- World
premiere of the interior of the new sleeping and couchette car
- Modern
design, greater comfort and privacy for travelers
- Total
of 33 next-generation Nightjets on the rails by 2025
ÖBB and
Siemens Mobility unveil the next generation of Nightjet sleeping and couchette
cars at the Siemens Mobility plant in Vienna. The new cars are designed to
optimally accommodate the needs of customers and score points with modern
design, greater comfort and increased privacy. By the end of 2025, a total of
33 next-generation ÖBB Nightjets will be on the rails, connecting European
cities overnight at speeds of up to 230 kilometers per hour in a
climate-friendly way. The first trains are scheduled to be in use by the end of
summer 2023 on the popular routes from Austria and Germany to Italy.
- 65 Vectron AC and Vectron MS
locomotives called from existing framework agreement
- Delivery includes locomotives with a
top speed of 230 km/h
- Milestone
reached: 1,500 Vectrons sold
Akiem, the
leasing rolling stock specialist company for rail vehicles, has ordered 65
Vectron AC and Vectron MS locomotives from Siemens Mobility. The order was
placed as part of a framework agreement for the purchase of locomotives that
was signed in December 2021. The first locomotives from this call are to be
delivered in mid-2024. Akiem previously ordered 20 Vectron locomotives from
Siemens Mobility last December.
- Delivery of 14 Vectron MS
multisystem locomotives
- MRCE fleet includes 147 Vectron
locomotives
Mitsui Rail
Capital Europe (MRCE), a full-service locomotive leasing company, has ordered
14 Vectron MS multisystem locomotives from Siemens Mobility on the basis of an
existing contract. With this order, MRCE will have a fleet of 147 Vectrons.
MRCE plans to use the locomotives in Germany, Austria, Hungary, Poland, the
Czech Republic, Slovakia, Romania, and the Netherlands.
InnoTrans 2022, September 20-23, 2022, Messe Berlin, hub27, booth 230
- Siemens Mobility presents Siemens Xcelerator, the open digital business platform
- Fair highlights: Next-generation hydrogen train Mireo Plus H; infrastructure in the cloud; 100% system availability with Railigent X; unique software portfolio Mobility Software Suite X
- Motto of the company’s show: “Destination Digital”
Siemens Mobility is presenting its new digital business platform Siemens Xcelerator at InnoTrans 2022. Siemens Xcelerator is an open digital business platform with the ambition to create a powerful ecosystem of partners who can jointly accelerate digital transformation and sustainability in mobility at scale. By opening interfaces for all participants of the mobility ecosystem, Siemens Xcelerator helps connect the real with the digital worlds – a first-of-its-kind innovation in the rail industry.
Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
- Latin America’s first fully automated metro line (GoA 4)
- Siemens Mobility digitalized CBTC technology installed across entire 15 km of track,11 stations, and 29 trains
- Automated signaling provides greater availability, enhanced operations, and passenger experience
ViaQuatro has successfully begun full operation of São Paulo’s entire Metro Line 4 with Siemens Mobility’s Communications-Based Train Control (CBTC) signaling. Since its first stretch opened in 2010, it has been the first fully automated metro line in South America that can operate with GoA 4, the highest grade of automation that allows trains to be automatically controlled and operated. The digitalized and optimized system allows for a more efficient and centralized control of operations, while also increasing the safety, availability, and capacity across the entire network.
Siemens Mobility has handed over the 100th ICE
4 to Deutsche Bahn. The train was christened “Rheinland-Pfalz” at the official
ceremony held in Mainz today, attended by Dr. Richard Lutz, CEO of Deutsche
Bahn AG, Dr. Michael Peterson, DB Board Member for Long Distance Passenger
Transport, Dr. Volker Wissing, Federal Minister for Digital Affairs and
Transport, Malu Dreyer, Minister President of Rhineland-Palatinate, and Dr.
Roland Busch, CEO of Siemens AG.
“We are pleased that the ICE 4 is the backbone of DB’s long-distance transport and thank our customer for their trust. Our trains help DB make rail transport more attractive and protect the environment. The fact that we have delivered 100 ICE 4s shows that we have the right portfolio for high-speed transport. Moreover, the ICE secures thousands of jobs in Germany,” said Roland Busch, CEO of Siemens AG.
DB will receive a total of 137 ICE 4 trains in various configurations by the end of 2024. In addition to the 50 12-car trains that have already been delivered, 19 of the 37 ordered 7-car trains are already in use, such as on the ICE line between Cologne and Berlin. 33 13-car XXL ICE trains, of which DB has ordered 50, have also been added to the fleet since February 2021. The 13-car trains have almost 1,000 seats, more than ever before in an ICE and five times more than in a medium-haul airplane. Siemens Mobility delivers a new ICE 4 every three weeks. At this rate, DB will be able to expand its capacity by another 11,000 ICE 4 seats by the end of this year.
Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.