- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
- In a pilot project, Siemens is combining its Sigreen emissions management software with BayWa Carbon Connect, BayWa’s software for emissions offsetting
- The real carbon footprint of products is made transparent across the supply chain, from emission generation and reduction to offsetting
- In an initial use case, Siemens is offsetting the carbon emissions of selected products of the Simatic S7-1500 family at the Electronics Works Amberg for the duration of the project
The technology company Siemens and BayWa AG are working together to advance CO2-optimized industrial production. As part of a pilot project, the two companies are combining Sigreen, Siemens’ software for emissions management, with BayWa Carbon Connect, BayWa’s software for emissions offsetting.
- Industrial Connectivity Lab opens at the Erlangen site
- Test environment for industrial connectivity technologies
- 5G, WLAN, RTLS, and RFID: Users test application scenarios and interoperability in industrial conditions
The technology company Siemens has opened a new test laboratory for industrial connectivity technologies at its Erlangen site. Embedded in the Siemens Technology Center on the Erlangen campus, the Industrial Connectivity Lab offers 300 square meters of space for extensive testing of any connectivity solution in industrial environments: Industrial WLAN, 5G, real-time localization systems (RTLS), and radio frequency identification (RFID).
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.
- Independent analyst firm has recognized Siemens Smart Infrastructure as a leader in integrated smart building security software
- The software is part of the Siemens Xcelerator portfolio
Industry analyst firm Verdantix has ranked Siemens Smart Infrastructure as one of the leading providers for security software in smart buildings. Their recently published “Green Quadrant: Integrated Smart Building Security Software 2023” report analyzes and evaluates ten companies that are shaping the market. Verdantix noted that Siemens solutions offer highly advanced unified security management capabilities. The assessed Siemens software is part of Siemens Xcelerator, an open digital platform that enables customers to accelerate their digital transformation.
- Collaboration to make industrial robotics more accessible and usable for manufacturing SMEs
- Exploration of new solutions to advance interoperability and more efficient interfaces between automation and robotics systems to address existing hurdles and cost drivers
- Solutions to speed up the development process for flexible work cells and facilitate their operation
Intrinsic, an Alphabet
company, and Siemens have teamed up to explore integrations and interfaces
between Intrinsic’s robotics software, which is designed for easy use of
AI-based capabilities, and Siemens Digital Industries with their open and
interoperable portfolio for automating and operating industrial production.
- Lighter, faster and more efficient aircrafts are needed to reduce emissions in aviation
- By leveraging Siemens Xcelerator – our open, digital business platform – companies achieve digital transformation easy, fast, and at scale
- With SINUMERIK ONE, our digital native CNC, aerospace manufacturers can take high-end part manufacturing to the next level
Aerospace industry has many challenges ahead:
cost pressure, changing market conditions, and society’s demand for sustainable
mobility. Automation and digitalization are helping airplane
manufacturers to take up these challenges and reach climate targets like ‘Fly
Net Zero’. Therefore, Siemens offers a wide range of solutions for aviation
along the entire value chain – from the concept and design until an aircraft is
ready for take-off and through end of service. Siemens portfolio consists
of design and simulation software, manufacturing automation and management,
robotics, composite solutions, intelligent building automation management
systems and lifecycle management software.
- Siemens Xcelerator portfolio used to develop the digital twin of the next generation of Maeve’s zero-emissions, all-electric aircraft
- Maeve 01 aircraft enables 44+ passengers to travel in a range over 250 nautical miles at significantly lower energy consumption compared to the previous generation
- Latest design aircraft reduces operating economics by 30% compared to existing turboprops
Siemens Digital Industries Software today announced
Maeve Aerospace B.V. has adopted the Siemens Xcelerator portfolio of industry
software and services to aid in the development of Maeve 01 – its next-generation,
zero emissions all-electric passenger aircraft. Unveiled at the Paris Air Show,
Maeve 01 enables 44+ passengers to travel in a range of 250nmi with zero
emissions.