Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

RRX regional trains inaugurates service on schedule

The picture shows the new electric multiple unit (EMU) train built by Siemens Mobility for the Rhine-Ruhr Express (RRX).

The picture shows the new electric multiple unit (EMU) train built by Siemens Mobility for the Rhine-Ruhr Express (RRX).

"With the commissioning and series approval of our Desiro HC train for the Rhine-Ruhr Express, we've once again demonstrated that we can deliver mega rail projects right on time. This makes us a reliable partner for transport companies worldwide when it comes to handling complex projects throughout their entire lifecycle," said Sabrina Soussan, CEO of Siemens Mobility.
The Rhine-Ruhr Express is the world's first series-produced train to feature a new high-frequency window treatment that vastly improves cellphone reception in trains. Researchers at Siemens Mobility developed this special window coating that allows radio signals to pass through the glass unhindered. The solution is a fine pattern that is lasered into the electrically conductive, transparent coating of the window panes. The installed windows allow radio waves to penetrate the glass up to 500 times better than with conventional thermal insulation glazing. With this special solution, passengers can surf in the Internet and phone for the first time without signal disruptions, and there is no need to install special in-train repeaters in the coaches.
Approval of the Federal Rail Authority was granted following the new procedure in Germany which gives train manufacturers and operators planning security. In this procedure, proof and test certificates can be issued by recognized testing centers beginning with the design phase of the train.
In North Rhine-Westphalia (NRW), around 2.4 million people use the regional rail system on a daily basis, and the numbers are growing. The RRX, which is acclaimed as a project of the century for the metropolitan region, will help meet the continually growing transport demands in the Rhine and Ruhr region. When completed, seven rail lines will connect major cities in NRW with important centers such as Kassel and Koblenz in the neighboring states of Rhineland-Palatinate and Hesse. On the core route between Cologne and Dortmund, passengers will be able to use rail services every quarter of an hour once the system's infrastructure has been expanded and modernized. The system will benefit eight million people living in cities providing RRX service, or around 45 percent of the NRW population. 
Siemens Mobility will be delivering a total of 82 specially developed double-decker trains from the proven Desiro train family. The newest family member, the Desiro HC, is designed for high passenger capacities. Each 105-meter train consists of four cars and has 400 seats. In operation, two train units will be coupled to create an eight-car express with around 800 seats. In addition, Siemens Mobility will be responsible for the service and maintenance of the trains over a period of 32 years. A state-of-the-art maintenance facility, the most modern in the world, was built specifically for this purpose in Dortmund-Eving. The RRX contract, with a volume of €1.7 billion, marks the biggest order Siemens Mobility has ever received for Germany's regional rail transport sector.

This press release, press photos and additional material are available at: www.siemens.com/press/RRX

For this press release

Feature: Billion-euro order: Siemens to build Rhine-Ruhr express

Feature: Billion-euro order: Siemens to build Rhine-Ruhr express

@SiemensMobility

@SiemensMobility

@SiemensMobility

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2018, which ended on September 30, 2018, the former Siemens Mobility Division posted revenue of €8.8 billion and had around 28,400 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more

Contact

Ellen Schramke

Nonnendammallee 101
13629 Berlin
Germany

+49 (30) 386-22370