Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

ICE 4 begins regular service

DB plans to reach its ambitious growth goals with the ICE 4 fleet. The operator's mainline strategy, approved in 2015, is to expand its long-distance offerings by 25 percent by 2030. DB wants to attract an additional 50 million passengers a year, and the ICE 4 will provide the backbone for its long-distance service.
"The ICE 4 is the new flagship for our long-distance routes and sets standards for our passengers: Plenty of storage space for luggage, an elegant restaurant and an innovative lighting concept ensure a high level of comfort for passengers. This is the first ICE on which passengers can take their bicycles. Thanks to a completely revamped family area and parent-and-child compartment, we're making journeys even more relaxing for families," says Birgit Bohle, Chairwoman of the Management Board of DB Fernverkehr AG.
"The ICE 4 is the biggest order for trains ever received in the nearly 170-year history of Siemens. We're right on schedule with the execution of the order, and regular service could be started punctually. This train sets new standards in intercity transport with its unique technological concept," explains Sabrina Soussan, CEO of the Mobility Division.
The ICE 4 trainset was designed to provide the greatest possible flexibility. A total of 24 train configurations are possible on the basis of five car types and the trains can be adapted to capacity requirements, top speed and the selected route profile. A prerequisite for the virtually freely configurable trains was the development of a so-called powercar that combines all traction components within a single car. In these powercars, all main traction and power supply components are arranged under the car floor. The trains are a combination of powercars, a service car, intermediate cars and two end cars. A 12-car ICE 4, for example, is driven by six powercars and can reach a top speed of 250 km/h.
The 346-meter long, 12-car train offers 830 seats and has large luggage racks located near the seats. A family compartment offers more room compared to earlier cars. The train also has additional open areas for accommodating baby buggies in the parent and child section. Four spaces are available for passengers in wheelchairs and, for the first time, it will be possible to take along bicycles in an ICE: eight spaces can be reserved in the end car.
An innovative lighting scheme is attuned to the time of day and creates a pleasant atmosphere inside the cars. The system provides subdued lighting in the early morning, and when the sun rises, it turns into a warm and stimulating tone before shifting to normal daytime lighting. In the evening, the lighting system simulates a setting sun.
A new type of air conditioning system ensures that outside temperatures ranging from a minus 25 degrees Celsius to a plus 45 degrees Celsius can be comfortably handled. The system is also redundant, so that one part will continue to operate if the other should shut down.
The new and modern seats have improved headrests. When adjusted, the seatbacks don't recline to the rear but rather into the seat's shell without disturbing the passenger behind. Each seat in 1st class has its own electrical socket and a reading lamp. Reservation signs and seat numbers are easily visible and reachable, and integrated into the seat headrests. The new trains have multi-provider technology using the latest WiFi technology. The system connects with the fastest data network available (LTE, 3G) while the train is underway and bundles the capacities of the network operator so that higher data volumes can be processed. This provides passengers with a faster and more stable WLAN connection.
The ICE 4 fleet is equipped with the European Train Control System (ETCS). With this system, the ICE 4 will be able to operate on the new high-speed rail route between Berlin and Munich as of December 2018.

This press release, press photos, film clips and additional material is available at: www.siemens.com/press/ice4
Further information on the Mobility Division is available at: www.siemens.com/mobility

For this press release

Feature: Largest order - Siemens is building ICE 4 trains for Deutsche Bahn

Feature: Largest order - Siemens is building ICE 4 trains for Deutsche Bahn

@SiemensMobility

@SiemensMobility

@SiemensMobility

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Ellen Schramke

Siemens AG

Nonnendammallee 101
13629 Berlin
Germany

+49 (30) 386-22370

Eva Haupenthal

Siemens AG

Werner-von-Siemens-Str. 1
80333 Munich
Germany

+49 (89) 636-24421