Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

First Vectron broad-gauge locomotives received authorization in Finland

First Vectron broad-gauge locomotives received authorization in Finland
For testing and certification of the extensive new equipment package for Finland, up to five locomotives have been undergoing type tests according to the Technical Specifications for Interoperability (TSI) since early 2016. Various additional functionalities and equipment packages were certified, such as the broad-gauge bogies, the special winter package and the two diesel power modules for bridging short stretches without an overhead power line.
The VR Group ordered the Nordic version of the Vectron in February 2014. The locomotives have a maximum output of 6.4 MW and a top speed of 200 km/h. The bogies are designed for operating on 1.524 mm broad-gauge lines. The locomotives will be used in Finland and are equipped with the European Train Control System (ETCS) as well as the Finnish JKV-STM train control system. The locomotives will have the series designation Sr3. The Vectrons are specially equipped to operate under harsh Nordic winter conditions in Finland, such as frequent collisions with larger animals, temperatures as low as 40°C below zero and powder snow. To handle these conditions, the locomotives are built with cavity roofs and a reinforced front hatch. Other special features include side buffers and automatic couplers.
Timber is frequently transported by rail in Finland and trains are moved in and out of forests on non-electrified rail lines. The Vectron accomplishes this with two diesel power modules and on-board radio remote shunting controls. With this system, there is no need for separate diesel shunting locomotives.

This press release and press photos are available at: www.siemens.com/press/Vectron-Finland
For further information about the Vectron locomotive, please see: www.siemens.com/press/vectron
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Ellen Schramke

Siemens AG

Nonnendammallee 101
13629 Berlin
Germany

+49 (30) 386-22370