-
Series
483/484 now running on S47
-
Ten
pre-series trains begin service in January
-
More
comfort and space for passengers
The New Year is starting off with a premiere! Shortly after midnight on
January 1, the first train of the new series 483/484 S-Bahn will start
passenger service in Berlin.
- The new series 483/484 trains are waiting to begin service – Premiere run on New Year’s Eve on line S47
The countdown for a new S-Bahn era has begun! Two weeks before their inaugural run on January 1, the new series 483/484 trains are ready and waiting to be deployed.
- On-time handover of 84
th and final train for the Rhine-Ruhr Express
(RRX)
- The RRX train offers highly innovative, digitally networked, and
high-performance mobility service for people in the Rhine-Ruhr region
- Digital maintenance ensures nearly 100-percent availability
The 84
th
train for the Rhine-Ruhr Express (RRX) infrastructure and mobility project was handed
over right on schedule. The trains were originally ordered from Siemens
Mobility in 2015. The RRX order, consisting of trains and a service contract,
has a total volume of €1.7 billion and marks the largest order received by
Siemens Mobility to date in the sector of regional rail passenger transport in
Germany.
- One single device for lines of up to 500 km
- Monitoring for powered, unpowered or grounded lines
- Highly precise localization of line faults
- Simplifies maintenance and increases network reliability
Siemens Smart Infrastructure recently launched its new PowerLink CM, a condition monitoring solution for high-voltage AC and DC transmission lines. To ensure reliable power supply, optimize grid utilization and prevent blackouts the device is designed to precisely locate faults in the transmission grid and continuously track line conditions. One single PowerLink CM device is sufficient to monitor line lengths of up to 500 km. Faults as well as line condition can be detected in powered, unpowered or grounded lines. Fault reports are received by the affected substation and are forwarded from there to the control room. For continuous line monitoring, the device can be connected to MindSphere, the open cloud-based Internet of Things (IoT) platform from Siemens, which facilitates transparent processing of all line data in the cloud. This allows grid operators to analyze status reports and optimize maintenance activities.
- Charging, medium and low-voltage technology for two carports at Hamburger Hochbahn AG’s Alsterdorf bus depot
- Space-saving installation as technical center on carport’s roof
- Important step for transitioning to climate-friendly local transport in Hamburg
Siemens Smart Infrastructure won a major contract from Hamburger Hochbahn, the largest local transport provider in the Hanseatic city. Siemens will equip two of the six carports at the Alsterdorf bus depot with a total of 96 charging points as well as medium and low-voltage technology. Operations are scheduled to start in summer 2021. With a total of 240 parking spaces, it is one of the largest and most modern bus depots for electric buses in Europe.
- First CBTC project in India with GoA 4, the highest grade of automation
- Will allow for trains to be automatically controlled and operated
- Automated signaling and train operations will provide greater availability and enhance operations and passenger experience
Siemens Mobility and Siemens Limited India is partnering with Bengaluru Metro Rail Corporation Limited (BMRCL) to implement a comprehensive set of automated train solutions for phase 2 of the Bengaluru metro expansion project. This will be the first CBTC project in India with GoA 4, the highest grade of automation that allows for trains to be automatically controlled and operated. Siemens Mobility will install its communications-based train control (CBTC) system across 18.8 km of the Yellow Line, which will feature electronic interlockings, an automatic train protection and supervision system, as well as a telecommunication system. The automated signaling and train operations will allow BMRCL to run trains 90 seconds apart, providing greater availability and an enhanced passenger experience.
- Grazia Vittadini from Airbus and
Kasper Rørsted from Adidas are being proposed to Siemens’ shareholders as new Supervisory
Board members
- Jim Hagemann Snabe to be nominated
again as candidate for Supervisory Board chair
- Proposals underscore importance of
diversity, sustainability and digitalization for Siemens’ Supervisory Board
- Election to be for a four-year term
in each case
Siemens is
proposing two candidates for election as new Supervisory Board members by its
shareholders at the Annual Shareholders’ Meeting on February 3, 2021:
Grazia Vittadini (51), Chief Technology Officer and member of the Executive
Committee at Airbus, and Kasper Rørsted (58), CEO of Adidas AG.
- Researchers from seven countries recognized for outstanding research
achievements and technologies
- Inventors come from all age groups and
all three Siemens companies
- Capacity for innovation remains high:
23 inventions per workday
- Investments of €4.9 billion in research
and development planned for fiscal 2021
For the 26th time, Siemens has recognized employees as Inventors of the Year to honor their outstanding research achievements. The 22 awardees from the three companies Siemens AG, Siemens Energy and Siemens Healthineers are from China, Germany, France, India, Israel, Spain and the U.S. Individual researchers as well as diverse research and development teams that work internationally were honored with the award.
- FIA and Siemens extend partnership to provide the ‘FIA Mobility Advocate’— a unique software and hardware toolkit — for FIA Mobility Member Clubs to strengthen advocacy of future transport solutions
As an
“Official Supplier of Urban Mobility Advocacy Solutions” for the Fédération Internationale de l’Automobile (FIA), the governing body of world motor sport and
the federation of the world's leading motoring organisations, Siemens plans to
develop a toolkit of software solutions for FIA Member Clubs to help them
provide an evidence-based approach to advocate for the implementation of mobility
policies and strategies. The ‘FIA Mobility Advocate’ combines modeling for
mobility, autonomous vehicles, and the environment, with enhanced analysis
outputs to help meet current future mobility goals.
- Sitrans CC240 IOT gateway provides standardized access to the lifecycle data of HART® devices
- Reduced service effort thanks to faster identification and removal of measuring and parameterization errors without additional parameterization tools
- Compatible with all OPC UA client applications
- Direct connection to Siemens MindSphere
- Numerous possible applications for on and off-premise solutions
Siemens presents the Sitrans CloudConnect 240: a new IOT gateway for the process industry. It provides a second data channel, completely independent of the control system, which is used to transmit data from any HART®-based field devices to the IT world.