- Digital twin of the machine, the workpiece, and the controller available in an end-to-end offering on Siemens Xcelerator Marketplace
- Siemens underscores its technology leadership in combining the real world with the digital world
- Less scrap and avoidance of machine damage
- Up to 40 percent faster production ramp-up of the machine
The technology company
Siemens, an innovation leader in automation and digitalization, and DMG MORI, a
leading global supplier of cutting-edge machine tools for turning, milling, and
grinding as well as for additive manufacturing, are presenting the first end-to-end
digital twin for machine tool machining on Siemens Xcelerator. Based on the
Digital Native CNC Sinumerik One, the offering includes the digital twin of the
controller, the customer-specific DMG MORI machine tool, and the workpiece and
is available now on Siemens Xcelerator Marketplace.
- Industry-defining digital twin for machine tool processing available in an end-to-end offering on the Siemens Xcelerator Marketplace
- Virtual machine and virtual CNC simulate milling of virtual part
- Efficiency gains include up to 40 percent faster ramp-up time
- Siemens and DMG MORI partnership underscores power of ecosystems
- Milestone marks another step toward industrial metaverse
Siemens AG and DMG MORI, global leaders in
automation and precision machine tools, are offering an industry-defining
digital twin for machine tool processing on the Siemens Xcelerator Marketplace.
Based on the Digital Native CNC (Computerized Numerical Control) Sinumerik One, this
offering encompasses a digital twin of the control system, the machine tool and
the workpiece, enabling breakthrough improvements in sustainability,
flexibility and time-to-market. CNC SINUMERIK ONE is the leading-edge control
system responsible for machining with machine tools.
- 106 new trains delivered on schedule and in passenger service
- New trains offer a high level of comfort, state-of-the-art passenger information and cameras for greater security
- Ceremonial delivery of last train of the new 483/484 series to enter service
The new Berlin S-Bahn fleet has been completed today: all 106 trains of
the new series are now in service. The trains, equipped with air conditioning, state-of-the-art
passenger information systems and cameras for greater security, offer passengers a new level of
comfort and convenience. The new fleet also increases the transport capacity in parts of the
city’s S-Bahn network, thus expanding services. In the course of replacing the older trains, the
number of cars per train was also increased. For customers, this has specific benefits: longer
trains operate on the Ring lines S41/S42 as well as the S8 line, and the S8 line is extended to
Wildau during peak hours. The new S-Bahn fleet now offers a total of around 18,000 seats. The
new trains have entered service successively since the beginning of 2021, and have been
operating on lines S41, S42, S46, S47 and S8 since then.
- Mireo Plus H hydrogen train reduces CO2
emissions on routes around Augsburg
- Passenger service starts in mid-2024
Siemens Mobility has
completed the first test runs with the Mireo Plus H hydrogen-powered train in
Bavaria. The two-car trainset will enter passenger service in mid-2024 on
routes between Augsburg and Füssen and Augsburg and Peissenberg on the rail
network of Bayerische Regiobahn (BRB). Pilot operations of the train are
planned for 30 months and are supported by the State of Bavaria. Siemens
Mobility and Bavaria signed the corresponding development partnership in 2021.
- Humanitarian assistance for those impacted by the Morroco earthquake and Liby flooding
- Companies will match every euro donatd by their people
- Siemens Caring Hands e.V. supports relief organizations on the ground
Siemens AG
and Siemens Healthineers have each provided €500,000 in immediate assistance to
mitigate the suffering of earthquake and flood victims in Morrocco and Libya
and to support rescue efforts. In addition, both companies have called on the
people they employ to make donations. Every euro contributed as part of this
donation drive will be matched.
- Sinumerik Ctrl-E in V6.22 with new functions for evaluating and reducing energy consumption
- Flexible HMI portfolio for multifunctional machine tools
- Perfect compatibility in use and programming for easy integration into the existing machine fleet
At this year's EMO, Siemens is expanding its range of products and services with the "Digital Native" CNC Sinumerik One. The new CNC generation from Siemens, which was launched on the market in 2019, comes with numerous innovations in software and hardware. With the new Sinumerik software version V6.22, there are new technology functions for the Sinumerik One that increase transparency in the machine, simplify operation, reduce machine wear, and increase performance. This leads to the optimal use of available resources, for example by reducing scrap and repairs. It also helps to increase machine productivity by minimizing idle and production times, for example.
- Industry
analyst firm recognizes Siemens for clear strategy, broad portfolio and
successful commitment to industrial metaverse
- Siemens
manager Virginie Maillard elected to the Metaverse Standards Forum’s board of
directors
Siemens is
the leading international provider in the growing industrial metaverse market,
according to the latest PAC RADAR from PAC, the renowned market research
company specializing in business software, IT services and digital
transformation. This rating is based on three aspects: a clear strategy, an
existing portfolio and the progress Siemens is making in this area.
- Framework agreement worth more than five billion
euros
- Further development of the
Mireo platform
- Expected
deployment in 2028
Siemens Mobility has won the tender for a framework agreement to deliver
up to 540 single-deck electric multiple-unit trains for Austrian Federal
Railways (ÖBB).
- Number of people in the company’s educational programs in Germany grows 15 percent: more than 1,500 apprentices and participants in work-study programs to start their careers at Siemens in 2023
- Almost all apprenticeships and work-study positions on offer focus on jobs in technical areas, including IT
- Siemens and FAU are cooperating for a new English-language master’s program in sustainability management
More than 1,500 apprentices and participants in work-study programs in Germany will start their careers at Siemens on September 1. Despite the scarcity of applicants in the country’s apprenticeship market, this number has significantly increased compared to the previous year (2022: 1,300; 15 percent increase). For a while now, there has been an imbalance between supply and demand on Germany’s apprenticeship market: At the start of August, more than 220,000 training positions were reported as vacant. However, only around 117,000 of the country’s young people are currently looking for an apprenticeship.
- Presentation of framework agreement with Siemens
Mobility worth €400 Million for further ETCS expansion
- ETCS enables shorter headways and greater reliability
Siemens
Mobility and ÖBB (Austrian Federal Railways) are digitizing the Austrian rail
network to further enhance the attractiveness of public transport. ÖBB is aiming
to double the capacity of Austria’s entire rail system by 2040 to cope with
increasing passenger numbers. This goal is now a bit closer: The most modern
technology for railway operations – the digital European Train Control System ETCS – has now been implemented and commissioned on the 57-kilometer route
between Linz and Vöcklabruck. The system controls distances between trains, as
well as their direction and speed in real time. This enables the route to carry
more passengers and freight, and ensures that the trains run more reliably,
punctually, and safely.