Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Industries Online

Well ventilated - Blast furnace blowers in South Korea modernized with Siemens technology

The international steel maker Posco is one of the world's largest steel producers. As part of its modernization work, the blower drives for the furnaces were fitted with new Siemens technology.

The international steel maker Posco is one of the world's largest steel producers. As part of its modernization work, the blower drives for the furnaces were fitted with new Siemens technology.

The optimization measures include the installation of three Simotics HV high-voltage motors and Sinamics frequency convertors on the existing blast furnace. Thanks to the new drive system for the blowers, Posco benefits from exceptionally high availability (99 percent), low maintenance costs, and short start-up times.

The optimization measures include the installation of three Simotics HV high-voltage motors and Sinamics frequency convertors on the existing blast furnace. Thanks to the new drive system for the blowers, Posco benefits from exceptionally high availability (99 percent), low maintenance costs, and short start-up times.

The international steel maker, Posco, is one of the world's largest steel producers. To ensure consistently high levels of steel production, the company has invested in modernizing the blowers on its blast furnaces at its main plant in Pohang using Siemens drive technology. Thanks to the new blowers Posco benefits from exceptionally high availability and efficiency, short start-up times, and low maintenance costs.
The optimization measures on the blowers include the installation of three Simotics HV high-voltage motors with an output of 49 megawatts each. They are part of the largest motors of their type installed in South Korea. The drive also includes four Sinamics GL150 medium-voltage frequency convertors.
High availability and low maintenance
The new drive system for the blower provides Posco with the benefit of an exceptionally high availability of 99 percent as well as reliable and efficient blast furnace blowers which improves the overall production. The blowers have a very short start-up time, are easy to use, and have lower maintenance costs. Close proximity to the customer and innovative Siemens technology were decisive factors in winning the contract. "Siemens is a reliable partner for us and is quickly on site whenever we need them," says Jeong Han Lee, Maintenance Team Manager at Posco.

 

MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947