Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Industries Online

Water reliably under control - Green water management using automation technology from Siemens

Belleaqua develops green water management systems, and relies on remote monitoring and automation solutions from Siemens.

Belleaqua develops green water management systems, and relies on remote monitoring and automation solutions from Siemens.

The Logo! 8 controller used is able to detect fault statuses, control the flow of wastewater, reduce repair costs and cut downtimes by means of continuous monitoring.

The Logo! 8 controller used is able to detect fault statuses, control the flow of wastewater, reduce repair costs and cut downtimes by means of continuous monitoring.

A pioneer in the field of water management, Belleaqua develops green management systems for industrial corporations such as logistics companies, as well as for local authorities and private households. To ensure that its solutions are not only reliable but also simple and convenient for customers to use, Belleaqua relies on remote monitoring and automation solutions from Siemens. The technology used is able to detect fault statuses, control the flow of wastewater, reduce repair costs and cut downtimes to a minimum by means of continuous monitoring.
Belleaqua is breaking new ground in the field of water management. The company produces secure water tanks and management solutions designed to meet the Certipro certification requirements of the Flemish organization Vito (Vision on a Technology for a Better World). "We had the first certificates on the Belgian market for a concrete wastewater system," recalls Belleaqua founder Jean-Pierre Depauw. One reason for the system's success was that it provided a complete one-stop solution from a single supplier, all the way from manufacturing to installation. At the heart of the water management solution is a Logo! 8 programmable logic controller (PLC) from Siemens.
Comprehensive possibilities
"Before we came across Logo! 8, we used a controller from a different manufacturer," recalls Depauw. "But it simply didn't offer either the reliability we required or sufficient scope." Logo! 8 opens up wide-ranging possibilities such as the early detection of faults and the provision of information on water quality. The logic module recognizes fault levels which indicate how serious the problem is, and independently determines whether a technician should be assigned for repairs. Logo! 8 also controls aeration of the tanks to optimize the growth of naturally occurring microorganisms. These important microorganisms are used by Belleaqua to break down wastewater contaminants.
Top marks for both technology and supplier
Belleaqua is highly appreciative of the improvements made possible by Logo! 8 and the Logo! CMR2020 communication module. The PLC it uses is ideally suited for remote monitoring, and its partnership with Siemens has also been highly beneficial. If problems arise, Siemens experts are available to Belleaqua with help and advice. "We have found Siemens reliable. We don't have a single LOGO! that hasn't replied or has gone wrong – compared to the previous PLC, where we had been having difficulties, so this is great," sums up Depauw.

 

MediaService application reports may be based on previously published Siemens technical articles.

Links

Contact

Ursula Lang

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947