Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Industries Online

The robots have it under control - Plant manufacturer relies on Siemens technology to automate robot cells

Krüger Industrieautomation GmbH (Krüger) specializes in building plants and robotics for small and medium-sized businesses.

Krüger Industrieautomation GmbH (Krüger) specializes in building plants and robotics for small and medium-sized businesses.

The company relies on Siemens control technology for end-to-end control of the robot cells which is independent of the robot programming.

The company relies on Siemens control technology for end-to-end control of the robot cells which is independent of the robot programming.

Integral functions such as safety functionalities reduce costs, increase safety for the operators, and enable rapid diagnosis in the event of disruption.

Integral functions such as safety functionalities reduce costs, increase safety for the operators, and enable rapid diagnosis in the event of disruption.

Krüger Industrieautomation GmbH (Krüger) specializes in building plants and robotics for medium-sized businesses. The company makes end-to-end use of Siemens control technology. This allows all of the robot cell components to be controlled and monitored independently of the robot programming. Ease of use also reduces commissioning times. Integrated functions such as safety functionalities also reduce costs, increase operator safety and plant efficiency, and enable rapid diagnosis in the event of disruption.
In smaller plants, Krüger uses Siemens Simatic S7-1200F fail-safe programmable logic controllers (PLC) while Simatic S7-1500F systems are used in more complex projects. Andreas Pfeifer, Head of Project Engineering at Krüger, summarizes the benefits of an S7-1200 PLC which is used, for example, to automate the robot cell in a current project with lifting devices and gripper solutions: "It gives us the option of controlling and monitoring all the components in the robot cell independently of the robot programming – in this instance, the end position sensors for querying the gripper position. In addition to this, all the communication between the robot and the welding machine is via a Simatic S7-1200F control using the Profinet ethernet standard."
Safety areas with flexible design
In addition to standard communication, the robot is also connected to the machine on a safety level using the Profisafe communications standard. Using the "Safe Operation" option allows the robot's actions to be limited to certain areas. This also allows the operator to use the control to block or release specific transfer paths either as required or depending on the machine status. This provides flexible safety areas for the robot and operator. All of the safety functions are available in the PLC and are displayed on a Simatic KTP700 Basic Panel. "This allows the customer to quickly diagnose faults all the way down to the channel fault," says Pfeifer.
Convinced in every respect
The engineering is completed in the TIA (Totally Integrated Automation) engineering framework portal. As the system is automated from end to end, the programmer does not have to switch between different software solutions and programming languages which saves time and effort. A Simatic ET 200SP I/O module also contributes to this by rationalizing and simplifying the wiring. Krüger's previous positive experience with Simatic S7-1200 systems means the company intends to use other functionalities of the fail-safe control in the future, for example, remote access through the webserver function. "This will enable us or the customer to do initial diagnostics from home or on the road using a computer or mobile phone," says Pfeifer.

 

MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947