Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Remote access – secure and efficient: Version 2.1 extends scope of functions of management platform for remote networks

Siemens is offering the new Version 2.1 for Sinema Remote Connect, the management platform for remote networks.

Thanks to the logging of "Security Events", user activities and potentially critical system events in the Sinema Remote Connect server become transparent. The logging process, which takes place locally in the Sinema Remote Connect server and centrally in the Syslog server, can be used for example to trace which user most recently made changes to the settings. With the Syslog connection, these logs are then transferred immediately and securely via Syslog TLS to higher-level monitoring and analysis systems such as Security Information and Event Management (SIEM).

Transparent, efficient, secure

Thanks to the UMC connection, administrators no longer have to create user accounts manually in the Sinema Remote Connect server. Instead, existing users and groups from central systems such as UMC or Active Directory can be incorporated. This reduces effort and ensures consistent transparency. With the new version, remote access is even more efficient, comfortable and transparent, especially for users who want to log into the Sinema Remote Connect system using their standard Windows login. Rights are easily assigned centrally, and all actions are logged by a central Syslog server.
MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947