Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Quick and flexible assembly - New plug-in connector for on-site assembly of industrial-grade cables

Siemens is extending its FastConnect cabling technology offer to include a new X-coded IE FC M12 Plug Pro connector.

Reliable network components are essential for the digital transformation of industry. In addition to direct use of pre-assembled cables, individual components are also being used directly on site for flexible assembly which can be individually adjusted to the preferred length to suit the application. These include the new X-coded IE FC M12 Plug Pro plug-in connector which allows customized cables with data rates of up to ten Gigabytes per second to be created quickly and easily. The cores in the eight-core IE FC TP cable are inserted into eight small openings in the plug and shortened to length and connected by the integral cutting and clamping technology when the two housing elements are closed together. The pre-assembled cables can then be used to form connections with Scalance XP-200 Industrial Ethernet Switches, Scalance W-700 IWLAN (Industrial Wireless LAN) Access Points, Simatic ET 200eco PN distributed I/O modules, or Simatic MV540 optical identification systems.
All network components are installed partially inside and partially outside control panels. The latter places particular demands on the components – not only on the active products installed but also on the passive components such as industry-grade cabling and plugs in copper and fiber-optic designs.
MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947