Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Professional crane operation – Siemens network technology ensures highly efficient operation at container port terminal

Gantry cranes are the logistical backbone of every container terminal – they must run reliably for a long time, and communicate with the warehouse management system quickly and securely.

The reliability of a crane network is largely dependent on being able to transmit transport orders quickly, smoothly, and tamper-proof to the respective crane. When building a new container port terminal, the client therefore relies on Siemens crane, automation, and network technology. The final expansion stage of the plant will have 42 fully automated stacking cranes interacting across three storage segments, each with seven storage blocks. Two cranes service each storage block. Manned straddle carriers which transport the containers connect the cranes and the storage blocks. Siemens RFID (Radio Frequency IDentification) technology is used to track the containers.

Core components of the network solution implemented with Siemens Professional Services are over 300 Scalance switches series X-500, X-300 and X-200 for the structured, largely redundant communication among more than 1,000 participants.

Separate networks for high reliability
Two physically separated networks were used for the automation applications and PC applications so that, for example, data-intensive camera surveillance does not affect other applications. Redundant ring structures and redundancy mechanisms such as the High Speed Redundancy Protocol (HRP) and Standby Coupling, Virtual Router Redundancy Protocol (VRRP) and Open Shortest Path First (OSPF) routing protocol achieve shortest reconfiguration times in the event of a fault – and thus the highest availability of the entire crane network.

Reliable solution with redundant ring structures
The hub of the three-level network solution is formed by Layer 3 Scalance XR552-12M routers – two of each connected to a redundant ring in the operator's data center. One pair is for networking the automation components and the other for PC-based applications. All four routers are connected via a Scalance S615 Industrial Security Appliance to the higher-level backbone of the operator network. The routers communicate with the subordinate, similarly ring-redundant block level – each made up of two series X-300 Scalance Layer 2 switches per block in separate VLAN (Virtual Local Area Network) segments. With four further X-300 and X-200 series switches for each crane, the number of installed Scalance devices increases to more than 300. The network has over 1,000 participants, each of which was allocated a unique IP address so that they can be quickly identified and addressed.
Easy handling all down the line
All the devices were intensively tested, pre-configured, and optimized before they were commissioned via Sinema Remote Connect (a management platform for remote networks) using the Scalance Firewall and a secure, on-site VPN (Virtual Private Network) connection. The management platform allows the Siemens experts to engineer the automation systems remotely in the TIA (Totally Integrated Automation) Portal engineering framework and to install firmware updates. Problems which occurred during the step-by-step commissioning were diagnosed and resolved using Sinema Server (software for network monitoring). This convenient handling is prompting the operator to consider using the Siemens solution in addition to existing tools.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (152) 22915052