Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

New reader with maximum sensor resolution – Siemens adds new Simatic MV560 X optical reader and powerful accessories to portfolio 

Like the Simatic MV560 U, the new Simatic MV560 X reader also features a scan mode, which can be used to separate image capture and image processing. A series of images is stored directly on the reader. This stored image series ensures reliable reading, even with fast-moving objects. In addition, the expanded memory improves diagnostics by providing larger amounts of diagnostic information, such as error images. This increases plant availability.

Modular, versatile and configurable
In addition to the new Simatic MV560 X optical reader, the portfolio for the entire Simatic MV500 series has been expanded to include a large number of high-performance, individually configurable accessories.  e-focus lenses are now available in five focal lengths, which automatically focus the  object to be captured, so that manual intervention by the user is not required. New, flexibly controllable ring lights have also been added. They switch automatically between different lighting variants. In addition, a large number of metal lens protection tubes in different lengths with an integrated optical filter concept in the area of the windshield are now also available for different lighting scenarios. 

Siemens is expanding its hardware portfolio for optical readers to include Simatic MV560 X with particularly high resolution of 5.3 megapixels.

Thanks to the modular design of the Simatic MV500 devices, the automatic focusing and  software-controlled selection of the illumination, an extremely wide range of image processing applications can be implemented easily and reliably – even under changing production conditions and in difficult light situations. Configuration via web-based management and integration into the TIA (Totally Integrated Automation) Portal facilitates configuration. One-button configuration for network parameters enables IP (Internet Protocol) addresses for a connected PC to be assigned automatically. Admin rights are not required here. One-button configuration for read parameters, by contrast, allows the read parameters, the lens focus, and the illumination to be automatically set directly on the device without opening the web-based management.
Since all MV500 devices feature a compact design and IP67 degree of protection (protection against the ingress of water and foreign bodies), they are ideal for use in confined spaces and in harsh industrial environments.

Easy connection to the cloud

The optical readers are connected to cloud applications via the Simatic S7-1500 controller and the CP1545-1 communications processor. In addition, connection is also possible via a new generation Simatic RF18xC/CI communication module and an Industrial IoT gateway such as Simatic CC716 (in preparation).  
MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (152) 22915052