Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
News18 November 2019Digital IndustriesNuremberg
MediaService Digital Industries Newsroom
Modern security management – Digital companies benefit from a new version of Network Management System

With the new version V1.0 SP1 of the Sinec NMS Network Management System, Siemens is offering even more opportunities for the management of large data volumes and complex network structures as well as an overview of security-related network topics.
As in all previous versions, Sinec NMS V1.0 SP1 complies with security directive IEC 62443 (directive, i.a. for user role management and system security through encrypted data transmission). The new features are firewall and NAT management. The firewall is configured via a graphic description of the permitted communication relationship in the network, from which the system automatically generates the corresponding device-specific policies. If no translation of IP addresses is required, firewall management can also be used independently of the NAT function. NAT, however, facilitates especially the connection of series machines with identical IP addresses to overlaid networks.
Automatic documentation
With the local documentation function, user activities are documented with a time stamp. This means that audit log entries can be retraced, providing considerable savings in time and effort, e. g. for audits, and also ensures the audit compliance of the data. The audit information is available for analysis by other central systems such as a Security Information and Event Management (SIEM) system via the Syslog interface in Sinec NMS. In addition to audit log entries on user activities, system events such as network alarms can also be forwarded via Syslog.
Links
MediaService application reports may be based on previously published Siemens technical articles.
Contact
Ursula Lang
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7947