Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Keeping it clean – Siemens technology ensures efficient processes in the food and pharmaceutical industries 

Packo Inox NV manufactures high-quality stainless steel systems for hygiene-sensitive production processes in the food and pharmaceutical industries.

The equipment developed by Packo must be able to cope with harsh industrial environments and to be integrated into higher-level systems. To this end, Siemens uses QR (Quick Response) coding to allow access to its measuring devices’ technical information. This simplifies subsequent transfer of documentation as well as the integration of devices into third-party subsystems. Another area in which Siemens technology is used is Packo’s CIP (Cleaning in Place) systems. Tanks, pipes, heat exchangers, and other elements are automatically cleaned without even having to open or disassemble the components.

Robust, reliable technology
Packo relies on Siemens process instrumentation solutions for reliable monitoring of temperature, and other process parameters. This includes the Sitrans F M MAG 6000 for measuring the flow, the analog Sitrans P compact pressure transducer, and the Sitrans TS300 for measuring temperature. What all products taken from the Sitrans portfolio have in common is that they can cope with high temperatures and the occasionally aggressive cleaning chemicals for years on end.

Fully automated processes
The cleaning processes – water prestage, hot detergent and water/steam main cycle, followed by cold water – all run completely automatically. Which system components are cleaned, for how long, and with what, or the dosage of cleaning agent are also controlled by Siemens automation components. The same applies to the control, operation, and monitoring of the systems. Packo also supplies dispensing units and storage tanks in addition to CIP systems, relying always on Siemens’ easy-to-integrate and efficient solutions.

For a high degree of standardization while having the option of being able to meet specific customer requirements, Packo has relied for many years on automation and process instrumentation solutions from Siemens.

For a high degree of standardization while having the option of being able to meet specific customer requirements, Packo has relied for many years on automation and process instrumentation solutions from Siemens.

MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (152) 22915052