Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

It just works –  Siemens automation in a concrete plant makes easy work of integrating third-party systems

Siemens automation and weighing technology is used in a Canadian concrete plant and allows smooth integration of third-party systems.

When storing the individual raw materials used to make concrete, the materials can sometime absorb water from the atmosphere or, alternatively, dry out. This consideration has a significant influence on the weight. This means that, when weighing out the raw materials, the water content of the materials must be known and this information must be passed on to the weighing electronics which can then adjust the process accordingly. Microwave sensors are used to measure the moisture in a new concrete manufacturing plant in Canada together with Siemens Siwarex WP231 weighing modules. In addition to the weighing module, a Simatic S7-1200 PLC (Programmable Logic Controller) controls the amount of water added to the material when mixing the raw materials depending on the water content as well as the entire automation process.

SIWAREX WP231

Everything works – it’s that simple

Apart from the Siwarex and Simatic components, the Siemens solution also includes the TIA (Totally Integrated Automation) Portal engineering framework for easy project engineering in the plant. The benefit of the Siemens solution includes the fact that components from third-party suppliers, such as the complete instrumentation in this instance, can be integrated into a system without any problems. In addition to this, the system displays the entire weighing process digitally which provides a high degree of transparency and traceability, making quality assurance easier and significantly increasing plant efficiency. Any information required from anywhere in the entire weighing process is available to employees in the control room or on local HMIs (Human Machine Interfaces) via Siwarex, as are diagnostic or error messages which can be quickly identified and dealt with. Manual calibrations are also a thing of the past, making handling easier and increasing accuracy. Last but not least, Siwarex can accommodate both analog and digital inputs and outputs for a range of different tasks.
MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947