Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Interdisciplinary cooperation – Collaborative solution makes it easy to generate simulation models

Simcenter System Analystis a collaborative solution that allows for the creation of industry-specific applications to drive system simulation models.

“The platform powered by Simcenter System Analyst is meant to pool different expertise domains and different systems engineers and enables teams that never collaborated to sit together and communicate on their engineering issues to find common solutions,” said Eric Chauvelier, Method and Simulation Manager for Hybrid and Electric Systems in the Test & Digital Department for Renault.

Focus on the essentials

Project engineers need a fast and easy-to-use solution to run multiple variant analyses to evaluate design options and balance mechatronic systems’ performances. With Simcenter System Analyst, project engineers can focus on these aspects without having to also worry about model generation. The solution can also expand system simulation model reuse to project teams, helping maximize return on investment. Project engineers benefit from a user-friendly interface with an industry-specific approach, which means that even those with no CAE (Computer aided Engineering) skills can create simulation models and multi-attribute analysis.

Simcenter System Analyst allows users to easily change the parameter set.

Simcenter System Analyst creates an architecture choice for multi-attribute analysis.

MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7947