Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
News24 February 2020Digital IndustriesNuremberg, Germany
MediaService Digital Industries Newsroom
Heat-resistant with very high range – Maintenance-free SmartLabel for extremely high temperatures
Siemens is expanding its Simatic RF600 portfolio for ultra high frequency products to include the heat-resistant, passive and maintenance-free Simatic RF682L SmartLabel.
Due to its properties, the Simatic RF682L is suitable for the direct Radio Frequency Identification (RFID)-supported identification of objects in production logistics with high temperature stress. This includes for example paint shops.
The SmartLabel operates on the basis of standard ISO 18000-63 and is suitable for worldwide use thanks to the broadband design. In addition to the high temperature resistance, Simatic RF682L also features IP67 protection rating (protection against the ingress of water and foreign bodies) for use in harsh industrial environments. The label can be read using RFID (Radio Frequency Identification) readers from the Siemens Simatic RF600 portfolio.
Links
MediaService application reports may be based on previously published Siemens technical articles.
Contact
Ursula Lang
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7947