Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Control technology in a magnetic field – Velan Group and Siemens rely on close cooperation for valve development

The Velan Group is a world leader in the design and production of cast and forged steel valves for the chemical and pharmaceutical industry.

Velan gets supplied by similar industries such as the OEM (Original Equipment Manufacturer) department of Siemens Process Instrumentation. It therefore makes sense for the two companies to work together on the development of new innovative valves. This has led to an equal partnership, which is producing valve solutions that meet for example even the strict requirements in terms of vacuum density (helium leakage test) specified by the XFEL (X-Ray Free-Electron Laser Facility) in Hamburg, Germany. In the concrete project, the values also had to pass the function test in the magnetic field – which is a challenge even for proven Siemens Sipart PS2 positioners. 

Problem-free use in a magnetic field
A system with external electronics was developed specifically for these applications. The system part mounted on the actuator comprises only the pneumatic components and the signal feedback for the actuator. The actual control electronics is installed separately in a 19-inch module rack and is therefore outside the magnetic field. The valve positioner itself behaves quite normally in the magnetic field and the positioner system based on Sipart PS2 passed the demanding test in an independent test lab in all three dimensions (two directions per axis). The solution therefore met the customer’s strict requirements without problems. 

For the implementation of complex valve solutions, Velan relies on its long-term partner Siemens.

With the Sipart PS2 positioner, the valve solution even passes the qualification and function test in a magnetic field of 100 milliTesla (mT = unit of measurement for magnetic flux density).

Links

MediaService application reports may be based on previously published Siemens technical articles.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (152) 22915052