Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

Clever energy management reduces consumption and costs – Siemens solution as part of the integrated plant management system

Pikolin S.L. is a leading mattress manufacturer in France and Spain when it comes to sleeping comfort.

With Simatic Energy Manager Pro, Pikolin achieves a high level of transparency in terms of energy consumption. The energy management system is based on the ISO 50001 standards (standard for creation of systematic energy management) and helps the company to reduce energy consumption considerably. Using Energy Manager and the Simatic ET 200SP AI Energy Meter, meters and consumers can be integrated into the standardized energy management system and new devices implemented with just a few clicks. The Simatic WinCC Scada (Supervisory Control and Data System) solution and the Simatic Energy Suite provide a future-proof solution for the optimization of production and maintenance. Pikolin benefits from huge savings in the consumption of electricity (14 percent) and natural gas (40 percent), which increases the efficiency of the entire production process.

To achieve transparent energy consumption, Pikolin relies on a flexible and future-proof energy management solution from Siemens.

With Siemens technology, Pikolin is saving 14 percent on electricity per square meter in the company and around 40 percent on natural gas per cubic meter in the production area.

Using Energy Manager and the Simatic ET 200SP AI Energy Meter, meters and consumers can be integrated into the standardized energy management system.

With Simatic Energy Manager Pro, Pikolin achieves a high level of transparency in terms of energy consumption.

Siemens provides Pikolin with a future-proof solution for the optimization of production and maintenance.

The Siemens solution for energy management is part of the integrated plant management system.

Contact

Ursula Lang

Digital Industries

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (152) 22915052